- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Downloading demos to my CYW920719Q40EVB-01 is very inconsistent. It fails a majority of the time. If the UART port is not explicitly set, it cannot find the device. If I set the UART in the target, I get the error:
15:02:08 **** Build of configuration Release for project 20719-B1_Bluetooth ****
"F:\\Packages\\WICED-Studio-6.2\\20719-B1_Bluetooth\\make.exe" wiced_bt_class.L3_SuperMux-CYW920719Q40EVB_01 download UART=COM9
Linking target ELF
OK, made elf.
..\..\43xxx_Wi-Fi\tools\ARM_GNU\Win32\bin\arm-none-eabi-objdump: section '.ordered' mentioned in a -j option, but not found in any input file
..\..\43xxx_Wi-Fi\tools\ARM_GNU\Win32\bin\arm-none-eabi-objdump: section '.aon' mentioned in a -j option, but not found in any input file
..\..\43xxx_Wi-Fi\tools\ARM_GNU\Win32\bin\arm-none-eabi-objdump: section '.pram_rodata' mentioned in a -j option, but not found in any input file
Call to L3_SuperMux_spar_crt_setup @ 002159d9
OK, made F:/Packages/WICED-Studio-6.2/20719-B1_Bluetooth/WICED/../build/L3_SuperMux-CYW920719Q40EVB_01-rom-ram-Wiced-release/A_20719B1-L3_SuperMux-rom-ram-spar.cgs. MD5 sum is:
6e82d92b536a9a624a4d5c728ba16f6b *../build/L3_SuperMux-CYW920719Q40EVB_01-rom-ram-Wiced-release/A_20719B1-L3_SuperMux-rom-ram-spar.cgs
--------------------------------------------------------------------------------
Patch code starts at 0x00270400 (RAM address)
Patch code ends at 0x0027ACD8 (RAM address)
Patch RW/ZI size 2936 bytes
Application starts at 0x00215768 (RAM address)
Application ends at 0x002159D8 (RAM address)
Patch code size 43224 bytes
Application RAM footprint 624 bytes
------
Total RAM footprint 3560 bytes (3.5kiB)
--------------------------------------------------------------------------------
Converting CGS to HEX...
Conversion complete
Creating OTA images...
Conversion complete
OTA image footprint in NV is 50584 bytes
Downloading application...
****Download failed ****
Trying baudrate 115200 Conn: PORT=COM9 BAUDRATE=115200
Trying baudrate 3000000 Conn: PORT=COM9 BAUDRATE=3000000
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Terminated with error
Failed to determine baud rate
Download failed. This WICED platform of the SDK only supports download to 207x9B1 devices.
Follow the instructions in the 20719-B1 README.txt for downloading the application.
15:02:23 Build Finished (took 14s.756ms)
Hitting reset or doing a recover (-> Sw1 -> Sw2 <- Sw2 <- Sw1) does not fix the problem.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
It seems that the board came broken. Uploading projects to other boards works fine. Specifically, the recover function on the original board does not work. It keeps running the prior program after recovery and does not accept new ones.
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
The download log just shows the last few messages in the console:
Trying baudrate 115200 Conn: PORT=COM9 BAUDRATE=115200
Trying baudrate 3000000 Conn: PORT=COM9 BAUDRATE=3000000
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Initialized
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Terminated with error
Failed to determine baud rate
(from download.log)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
It seems that the board came broken. Uploading projects to other boards works fine. Specifically, the recover function on the original board does not work. It keeps running the prior program after recovery and does not accept new ones.