Hello,
I'm trying to program CYW920719Q40EVB-01 serial flash using the UART interface from my custom software. I'm using "WICED-HCI-Control-Protocol.pdf" documentation.
Also i have download log generated by using the download feature of the Wiced Studio 6.0 - ChipLoad.
I send the following sequence of commands (as described in documentation and which i see in Chipload mode) in recovery mode (recovery hold + push reset + release recovery) :
1) HCI_RESET: 01 03 0C 00
2) DOWNLOAD_MINIDRIVER: 01 2E FC 00
3) Parse uart.hex and send WRITE_RAM: 01 4C FC nn xx xx xx xx yy yy yy yy ....
4) LAUNCH_RAM to Address 0x00220000: 01 4E FC 04 00 02 22 00
where 0x00220000 is the first download address in the uart.hex file
5) CHIP_ERASE: 01 CE FF 04 EF EE BE FC (as in document)
6) Parse wiced_app.hex file and send WRITE_RAM: 01 4C FC nn xx xx xx xx yy yy yy yy ....
7) LAUNCH_RAM to Address 0xFFFFFFFF: 01 4E FC 04 FF FF FF FF (as in document)
When i try to download my wiced_app.hex WITH minidriver parsing i get an error on 6) step. I receive a wrong response from the board to first WRITE_RAM command:
Sending HCI Command:
0000 < 01 4C FC 46 00 00 50 00 42 52 43 4D 63 66 67 53 >
0010 < 00 00 00 00 32 00 00 00 01 01 04 C0 5D 00 00 00 >
0020 < 03 06 41 3E 19 9B 71 20 00 01 1C 00 40 50 00 00 >
0030 < 20 58 00 00 20 50 00 00 30 50 00 00 10 00 00 00 >
0040 < 00 00 00 00 00 00 00 FE 00 00 >
Received HCI Event:
0000 < 04 0E 04 01 CE FF 00 >
Failed to send hex portion at 0x00500000
Without minidriver parsing and CHIP_ERASE the application parsing passed but i get an error on 7) step. I receive a wrong response from the board to LAUNCH_RAM command:
Sending HCI Command:
0000 < 01 4E FC 04 FF FF FF FF >
Received HCI Event:
0000 < 04 0E 04 01 4E FC 12 >
Failed to send launch RAM
Also sometimes the board doesn't send any response in recovery mode for WRITE_RAM command.
Could you give me some advice that I could try to do with my Bluetooth board?
Solved! Go to Solution.
Hi,
Your host is your PC running you custom download software.
I have gone through the logs (my_program_log.txt.zip). The process is breaking at chip erase step.
I would suggest you to wait few seconds after issuing chip erase HCI command. Once the chip erase command is issued, the host will need to wait for several seconds until the memory is erased. During this wait time, the device will keep sending periodic (about once a second) progress report messages made up of bytes FF 01 CE. This message is an indication that the erase process is progressing. Once the erase is completed successfully, the device will send bytes
0E 04 01 CE FF 00.
Thanks,
-Dheeraj