- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi all,
I'm new to this community , and this is my first discussion, so thanks for this chance.
I have an eval board : CYW920706WCDEVAL, and I'm able to flash it with WICED correctly, but I need to attach it to Linux with hciattach command,
I was able to attach it but I don't know what I'm doing wrong now, because it was a long time since I did it.
Here is what I did for flashing :
- Press and Hold on Recovery button
- Press on reset for at least 1 seconds
- Release recovery after releasing the reset button
- Select demo.hci_uart_spi_bridge-CYW920706WCDEVAL TRANSPORT=SPI download example and start flashing the board.
By the way, here is the switch configs for the flash :
SW5 |
---|
P2 OFF |
P33 ON for RX |
P0 OFF |
P31 ON for TX |
P3 ON for CTS |
P30 ON for RTS |
For SW7 all first 5 are ON for SERIAL FLASH ENABLE |
Output of flashing : |
---|
Converting CGS to HEX... Conversion complete Creating OTA images... Conversion complete OTA image footprint in NV is 70235 bytes Detecting device... Device found Downloading application... Download complete Application running |
But when I execute hciattach to attach the module as HCI device with this command :
- hciattach -s 115200 ttyWICED_HCI_UART12 any
I did check that ttyWICED_HCI_UART12 is present in /dev for Cypress. And I got a device with zero MAC address :
hciattach command output: |
---|
hci1: Type: Primary Bus: UART BD Address: 00:00:00:00:00:00 ACL MTU: 0:0 SCO MTU: 0:0 DOWN INIT RUNNING RX bytes:0 acl:0 sco:0 events:0 errors:0 TX bytes:12 acl:0 sco:0 commands:3 errors:0 |
I even tried to restore the switches to default state :
SW5 : same as flash except RTS and CTS are off , and SW7 all OFF , and it didn't work with the default combination.
What should I do ?
Thanks, Talel
Solved! Go to Solution.
- Labels:
-
ispn:38625:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Problem solved:
- Plug EvalBoard into PC
- Set RTS and CTS ON on SW5
- Set first 5 pins on SW7 ON for serial flash
- Open WICED
- Set board to recovery mode : Hold Recovery -> +1s Reset -> Release Reset -> Release Recovery.
- Choose and double click on project : hci_serial_gatt
- Firmware downloaded correctly
- Reset SW5 and SW7 to default : SW5(Only RX and TX) SW7 (All OFF)
- Plug EvalBoard into Linux
- Attach it : sudo hciattach ttyUSB(X) -t 10 any 115200 noflow nosleep
- Module attached correctly with a good MAC address
- Now you can use BlueZ commands on it (Example: hciconfig, hcitool , ...)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Talel,
Can you try keeping following switch configuration:
P2- OFF
P33- ON
P0- OFF
P31- ON
P2, P33- OFF
SW7:
1-5 ON, others OFF
Make sure your HCI UART is not open anywhere else. Recover and then program the board.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Thanks for the reply,
I don't know why you mentioned the P2 and P33 again , is it a mistake ?
Any way I switched P3 and P30 OFF , and followed your combination , but WICED stuck at "Detecting device...".
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi BeTa_4607436 ,
If you were able to program from WICED correctly , it means HCI UART configuration is correct. So hciattach also should work. Make sure you have not opened / using HCI uart by any other console by mistake.
Also please refer Running BlueZ on CY Part if this will be helpful.
Regards,
Anjana
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I tried everything , I tried witch serial flash switch configuration , and a default switches config, with hciattach command from your link :
sudo hciattach /dev/ttyUSB15 -t 10 any 115200 noflow nosleep
it says "Device setup complete" , but no MAC address in the new HCI module.
And no other HCI uart is opened by other console.
Here are 2 switches combination I tried:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Can you try following switch configuration-
Can you first try programming the board using WICED SDK on Windows? Or you can try using Chipload- Programming Using Chipload.exe - KBA228316 to make sure there is no problem with hardware.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm using WICED under Linux, and I don't have Windows for the moment, I set the switch config as you requested,
WICED can detect the device but cannot download the binary, here is the log :
Converting CGS to HEX...
Conversion complete
Creating OTA images...
Conversion complete
OTA image footprint in NV is 70235 bytes
Detecting device...
Device found
Downloading application...
********* Download Failure *************
+------------------------------------------------------------------------------------------+
| Power cycle the CYW920706WCDEVAL board and retry. |
| If this problem persists, the serial flash on the board may be corrupted. |
| Please see Appendix D in the Kit Guide for recovery instructions. |
+------------------------------------------------------------------------------------------+
Download failed. This WICED platform of the SDK only supports download to 20706A2 device.
The project I'm trying to install is : demo.hci_uart_spi_bridge-CYW920706WCDEVAL TRANSPORT=SPI download
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Talel,
Can you try programming demo.hello_sensor project for now?
hci_uart_spi_bridge application acts as UART-SPI bridge which is needed for different audio applications like hci_audio_remote_control.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
It also failed to download, I don't know actually what is the problem, is there a problem with the hardware ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
If the switch positions are correct and you are recovering the board before programming then I dont think there should be some problem with board.
One thing you can try is recover and try downloading an empty project to the board.
Or if possible, if you get any Windows system then it will be easier to verify the exact problem.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Problem solved:
- Plug EvalBoard into PC
- Set RTS and CTS ON on SW5
- Set first 5 pins on SW7 ON for serial flash
- Open WICED
- Set board to recovery mode : Hold Recovery -> +1s Reset -> Release Reset -> Release Recovery.
- Choose and double click on project : hci_serial_gatt
- Firmware downloaded correctly
- Reset SW5 and SW7 to default : SW5(Only RX and TX) SW7 (All OFF)
- Plug EvalBoard into Linux
- Attach it : sudo hciattach ttyUSB(X) -t 10 any 115200 noflow nosleep
- Module attached correctly with a good MAC address
- Now you can use BlueZ commands on it (Example: hciconfig, hcitool , ...)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you for sharing the solution steps with us Talel.!