CYW20735 SPI issue

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
JoDo_4436536
Level 1
Level 1

Hello,

I am trying to bring up a similar (simpler) SPI master test program on 20735-B1, based on the SPI master example on 20719. My SDK version is 6.4.

Some code snippet:

    wiced_hal_gpio_select_function(WICED_P38, WICED_SPI_1_MOSI);

    wiced_hal_gpio_select_function(WICED_P07, WICED_SPI_1_CLK);

    wiced_hal_pspi_reset(SPI1);

    wiced_hal_pspi_init(

        SPI1,

        SPI_MASTER,

        0, 

        spi_master_get_gpio_cfg(WICED_P07, WICED_P38, WICED_P06),

        2.4*1000000,

        SPI_MSB_FIRST,

        SPI_SS_ACTIVE_LOW,

        SPI_MODE_0,

        WICED_P26

    );

uint8_t to_send[10] = {0x55,0x55,0x55,0x55,0x55,0x55,0x55,0x55,0x55,0x55};

wiced_hal_pspi_tx_data(SPI1, 10, to_send);

I've hooked up CLK and MOSI to an oscillator.

The CLK signal is as expected. However the MOSI output is definitely not 0x55.

Picture of sending one byte 0x55:

IMG_1543.JPGIMG_1544.JPG

As you can see in the above pictures, sending the same byte 0x55 results in different wave forms.

I wonder if there is any additional configurations needed for WICED_P38 port. Or I am missing some other software setups.

I've also tried an older revision of 20735 board using WICED 4.1. Same result.

0 Likes
2 Replies
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hi John,

Are you using CYW20735 EVAL or custom board?

Can you please try the below pin combination?

#define CLK                                  WICED_P07

#define MISO                                WICED_P16

#define MOSI                                WICED_P06

#define CS                                    WICED_P38

Thanks,

Anjana

0 Likes

Hi Anjana,

Thank you for your reply. Yes I am using the CYW920375Q60EVB-01 eval board.

I've tried your combination:

Code copied from 20719:

uint32_t spi_master_get_gpio_cfg(uint8_t clk, uint8_t mosi, uint8_t miso)

{

    uint32_t spiGpioCfg = 0;

    spiGpioCfg |= (clk << 16);

    spiGpioCfg |= (mosi << 8);

    spiGpioCfg |= (miso);

    return (spiGpioCfg);

}

spi_master_get_gpio_cfg(WICED_P07, WICED_P06, WICED_P16),

// configure led strip

    wiced_hal_gpio_select_function(WICED_P06, WICED_SPI_1_MOSI);

    wiced_hal_gpio_select_function(WICED_P07, WICED_SPI_1_CLK);

    wiced_hal_pspi_reset(SPI1);

    wiced_hal_pspi_init(

        SPI1,

        SPI_MASTER,

        0,

        spi_master_get_gpio_cfg(WICED_P07, WICED_P06, WICED_P16), 

        2.4*1000000,

        SPI_MSB_FIRST,

        SPI_SS_ACTIVE_LOW,

        SPI_MODE_0,

        WICED_P38

    );

It produces the same oscillator results as I showed above. The clock signal from P07 is correct. While the MOSI data from P06 is not 0x55.

0 Likes