Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

mawu_4270096
Level 5
Level 5
5 sign-ins First like received First like given

Hi :

    最近在使用CYW20735 RTC 模块遇到一些问题

   1. 根据CYW20735技术手册说明,如果使用外部32K晶振作为RTC时钟源,需要通过API去指定

     RTC使用的时钟源,但是并没有找到这样的API函数,目前使用内部晶振作为时钟源,RTC的误差

    很大,手册上面也说了,误差达到20%-30%

    2. 由于CYW20735是内部自带的RTC模块,所以如果想保持RTC时间正确,必须给RTC部分电路提供

备用电池,并且CYW20735模块断电,电池只能给RTC部分的电路供电,功耗必须足够低

   3. 使用RTC只要是对网络里面设备进行时间的同步,也就是需要用到time server  model与time client model

thanks!

mandy

0 Likes
1 Solution
Owen_Zhang123
Moderator
Moderator
Moderator
500 solutions authored 250 sign-ins 1000 replies posted

如果要获取高精度的RTC,必须使用外部32k时钟,系统在上电的时候会自动检测是否有外部时钟,如果有就会使用外部时钟,否则就使用内部LPO。

View solution in original post

0 Likes
3 Replies
Owen_Zhang123
Moderator
Moderator
Moderator
500 solutions authored 250 sign-ins 1000 replies posted

如果要获取高精度的RTC,必须使用外部32k时钟,系统在上电的时候会自动检测是否有外部时钟,如果有就会使用外部时钟,否则就使用内部LPO。

0 Likes

请问RTC供电问题怎样解决?一般的RTC模块都需要纽扣电池,如果使用CYW20735自带的RTC,怎样连接纽扣电池,是模块断电的时候,通过纽扣电池保持RTC的时间

0 Likes

这个设备没有办法单独给RTC模块供电,需要给这个设备供电才能保证RTC正常运行。

0 Likes