Hi,
I'm trying to output a clock on a GPIO pin but having zero luck!
This is the test code:
wiced_hal_gpio_select_function(WICED_P29, WICED_ACLK_0); // line 1
//wiced_hal_gpio_configure_pin(WICED_P29, GPIO_OUTPUT_ENABLE, GPIO_PIN_OUTPUT_HIGH); // line 2
wiced_hal_aclk_enable(1000000, ACLK0, ACLK_FREQ_24_MHZ); // line 3
I have tried with line 2 both commented and not commented and tried ACLK_1, ACLK_FREQ_1_MHZ and many different output frequencies but nothing works.
If the GPIO is configured as an output and toggled as fast as possible I can see this on the scope so my test environment is OK.
Please help!
Solved! Go to Solution.
Hi,
The issue is fixed for WICED SDK 6.4
The SDK should release in couple of weeks.
Currently we are tracking to get achieve before this month end.
Thanks,
Anjana