Hi,
I have connected a microphone via i2s on the CYW920719 board.
Is the only way to reroute the audio output from the microphone to A2DP through wiced_audio_start() and setting the route to AUDIO_ROUTE_I2S?
Also, is there a way to sample the microphone digitially (it is a 24-bit microphone) as hex or bytes?
Thanks so much in advance!
Solved! Go to Solution.
Hello,
Yes, I2S interface can be only used by A2DP . There is no other way.
Please have a look at blog here: https://community.cypress.com/t5/Resource-Library/PCM-I2S-Clock-setting-in-CYW20706/ta-p/246335
Q: Is the only way to reroute the audio output from the microphone to A2DP through wiced_audio_start() and setting the route to AUDIO_ROUTE_I2S?
A: Please have a look at watch demo example available in SDK
Note: Hope you also know that 20719 only supports A2DP source. Not A2DP sink.
Regards,
Anjana
Hello,
Yes, I2S interface can be only used by A2DP . There is no other way.
Please have a look at blog here: https://community.cypress.com/t5/Resource-Library/PCM-I2S-Clock-setting-in-CYW20706/ta-p/246335
Q: Is the only way to reroute the audio output from the microphone to A2DP through wiced_audio_start() and setting the route to AUDIO_ROUTE_I2S?
A: Please have a look at watch demo example available in SDK
Note: Hope you also know that 20719 only supports A2DP source. Not A2DP sink.
Regards,
Anjana