Hello,
I've been dealing with this strange problem since starting out on the CYW20719: declaring a global variable of class type leaves it uninitialized and unusable.
if I have this code for example in main.cpp:
class A {
public:
A(int val) : a(val) { WICED_BT_TRACE("A()"); }
int a;
}
A a = A(5);
APPLICATION_START() {
WICED_BT_TRACE("%d\n", a.a);
}
The constructor of A never actually gets called. How can I fix this?
Thank you,
Nicholas
Solved! Go to Solution.
Hi Nicholas,
Currently the WICED SDK does not fully support C++ and also we do not have any plan to support C++ in near future.
-Gyan
Hello Nicholas,
Could you please share your complete project files and steps to reproduce the issue which will help us to resolve the problem quickly ?
-Gyan
Hello Gyan,
I cannot share my complete project, but I will upload a minimum example today.
Nicholas
Hello gyan,
Here is a small example of my problem:
main.cpp:
extern "C" {
#include "sparcommon.h"
#include "wiced_bt_trace.h"
}
// Needed to have a base class?
void operator delete(void* ptr, unsigned int n) {}
class Base {
public:
virtual ~Base() {};
virtual void test() {
WICED_BT_TRACE("Hello");
}
};
class A : public Base {
public:
A(int* b) : b(b) {
WICED_BT_TRACE("A(%d)\r\n", *b);
}
void do_a() {
WICED_BT_TRACE("Doing %d\r\n", *b);
}
virtual void test() {
Base::test();
WICED_BT_TRACE(", world!\r\n");
}
private:
int* b;
};
// a1's ctor is never, called, and so using it will result in crashes
int bVal = 6; // primitives are initilized normally
A a1 = A(&bVal);
void test_a(A* a) {
WICED_BT_TRACE("Trying A*: ");
a->do_a();
}
void test_base(Base* base) {
WICED_BT_TRACE("Trying Base*: ");
base->test();
}
APPLICATION_START()
{
wiced_set_debug_uart( WICED_ROUTE_DEBUG_TO_PUART );
WICED_BT_TRACE("---------- Starting App ----------\r\n");
a1 = A(&bVal); // Assigning to the global will "kind of" initialize it, but passing pointers to the object fails
//A a2 = A(&bVal); // using a2 instead will make everything work
test_a(&a1);
test_base(&a1);
WICED_BT_TRACE("---------- finished ----------\r\n");
}
makefile.mk:
APP_SRC += main.cpp
C_FLAGS += -DWICED_BT_TRACE_ENABLE
Let me know if any other files/info is needed.
Thank you,
Nicholas
Hi Nicholas,
Currently the WICED SDK does not fully support C++ and also we do not have any plan to support C++ in near future.
-Gyan