Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

user_2209051
Level 1
Level 1
First like given Welcome!

Hi,

     i want to conn more devices via 20706,at least 10.But when 20706 ready to conn to the 7th device,func wiced_bt_gatt_le_connect return the status 0x85, WICED_BT_GATT_ERROR.
     i don‘t know how to break this limit.

     And my project conn params below
     min conn                       160ms
     max conn                      175ms
     slave latency                 3
     supervision timeout       10s

thx in advance!

0 Likes
1 Solution
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hi,

Not sure if the issue got resolved.

The no: of devices you can connect will depend upon your application , memory constraints , connection parameters etc.

You may also refer to following thread: Re: Maximizing number of connections with CYW20706

Thanks,
Anjana

View solution in original post

2 Replies
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hi ,

Can you provide the below details:

1: Which project are you testing? Any of our demo project or custom? Can you please share the project

2: When you try to connect 7th device, all other 6 devices are maintaining connection?

3: Can you please confirm if your application have enough  memory ?

4: What is the peer device which you are trying to connect? Are you getting a connection request at the peer side?

5. What is the max links configured in your project?

Thanks,
Anjana

AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hi,

Not sure if the issue got resolved.

The no: of devices you can connect will depend upon your application , memory constraints , connection parameters etc.

You may also refer to following thread: Re: Maximizing number of connections with CYW20706

Thanks,
Anjana