- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
SW Information
- Chipset & EVK : CYW20706 & F1DC2076 EVB (made in F1media)
- WICED SDK version : WCIED 6.2.1
- Test application : SPP
Test
- i have changed the transport to UART
- and i added the "wiced_sleep_config( WICED_TRUE, WICED_WAKE_GPIO_ACTIVE_LOW, WICED_WAKE_GPIO_ACTIVE_LOW );" to "end of APPLICATION_START()"
- and i was set the "BT_DEV_WAKE" pin to high
- and then current is lower than about 4 ~ 5mA
- "BT_HOST_WAKE" is keep to high, not changed to low
- i have tried to connect from phone to CYW20706
the "BT_DEV_WAKE" and "BT_HOST_WAKE" is as below.
the result of test is CYW20706 can not received the connection.
it seems that entered sleep mode, but can not wakeup.
i found that CYW20706 can be wake by BT Radio as below, but it was didn`t.
can CYW20706 wakeup by BT radio? why can not wakeup the CYW20706 by BT radio?
Solved! Go to Solution.
- Labels:
-
WICED Studio Bluetooth
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Could you please try using it as a standalone device and check the low power mode? Meaning, try using an external GPIOs instead og BT_Wake and Host_wake pins. General purpose GPIO can be configured and these interrup shout wake up the device.
BT Activity can also wake up the device. But I hope it will be in effective only after the connection. Before the connection the BT Device has to initiate the BT activity (Eg. using a timer or so) then it will wake up from sleep.
Thanks,
-Dheeraj.P.K