CYW20706 adc interface

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
duli_3411451
Level 1
Level 1
First like given

I saw CYW920706 have an ADC interface,can this ADC be used as analog MIC input?

Another question is if I got an I2s interface Micphone,Can I connect it to CYW920706‘s I2s interface directly?

0 Likes
1 Solution
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hi duli_3411451

Adding to BoonT_56 response.

Please note the I2S clock of CYW20706 can’t be set by the application directly. There is no API allowing the app to control the I2S bus. The FW configures it (as a Source or Sink) during A2DP Stream.

Refer PCM/I2S Clock setting in CYW20706

So if you are using A2DP profile in your application , then only you can connect the I2S codec / Mic to 20706 I2S and make it function.

Also while selecting the codec / Mic please select appropriately. The I2S is always configured for 16 bits per samples, Stereo

Thanks,

Anjana

View solution in original post

2 Replies
BoonT_56
Employee
Employee
500 likes received 250 likes received 100 likes received

You should connect the microphone to the I2S bus. If you are using the eval board, then you can connect directly

to the input pin at J22 Pin 7, see below.

WICED Studio Bluetooth Forums

0 Likes
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hi duli_3411451

Adding to BoonT_56 response.

Please note the I2S clock of CYW20706 can’t be set by the application directly. There is no API allowing the app to control the I2S bus. The FW configures it (as a Source or Sink) during A2DP Stream.

Refer PCM/I2S Clock setting in CYW20706

So if you are using A2DP profile in your application , then only you can connect the I2S codec / Mic to 20706 I2S and make it function.

Also while selecting the codec / Mic please select appropriately. The I2S is always configured for 16 bits per samples, Stereo

Thanks,

Anjana