What's the memory layout of the CYW20706?
Solved! Go to Solution.
There is a .ld file located in the build/project_name/spar_ram_proc.ld file which may helpful for the Ram address allocation.
The path in my PC: xx\WICED-Studio-6.0\20706-A2_Bluetooth\build\a2dp_sink-CYW920706WCDEVAL-rom-ram-Wiced-release\spar_ram_proc.ld
For NVRAM allocations, please refer to the doc located at \Doc\WICED-Firmware-Upgrade-Library.pdf
Regards
Jenson
Please refer to the doc located at \Doc\WICED-Firmware-Upgrade-Library.pdf
Here attached the recommended memory layout for external 4Mb memory:
I'm looking for the complete memory table, including internal RAM address allocations
There is a .ld file located in the build/project_name/spar_ram_proc.ld file which may helpful for the Ram address allocation.
The path in my PC: xx\WICED-Studio-6.0\20706-A2_Bluetooth\build\a2dp_sink-CYW920706WCDEVAL-rom-ram-Wiced-release\spar_ram_proc.ld
For NVRAM allocations, please refer to the doc located at \Doc\WICED-Firmware-Upgrade-Library.pdf
Regards
Jenson