- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I am using a CySmart BLE 4.2 dongle to detect and connect to my CVBT-42302802 module. I am using BTSpy.exe and ClientControl.exe with the appropriate trace messaging in my WICED application configured for WICED_ROUTE_DEBUG_TO_WICED_UART. When the CySmart dongle requests pairing, I get the following messages at the end of the pairing process.
14:15:25.541 SENT [1] Command to HCI. Name: HCI_LE_Add_Device_To_Resolving_List_Command (Hex Code: 0x2027 Param Len: 39)
14:15:25.541 Peer address type : Public (00)
14:15:25.541 Peer address : 00-a0-50-50-43-20
14:15:25.541 Peer irk : 73 46 13 95 95 c0 b4 1e 49 7b bd e3 65 f4 2d 0a
14:15:25.541 Local irk : 08 4e 9d 21 4c e2 6c 35 8c 4e 47 4d 3e 9f d1 9c
14:15:25.543 RCVD [1] Event from HCI. Name: HCI_Command_Complete (Hex Code: 0x0e Param Len: 4)
14:15:25.543 Num HCI Cmd Packets : 1 (0x01)
14:15:25.543 Cmd Code : 0x2027 (HCI_LE_Add_Device_To_Resolving_List_Command)
14:15:25.543 Status : Success (0x00)
14:15:25.545 SENT [1] Command to HCI. Name: ?? Unknown ?? (Hex Code: 0x204e Param Len: 😎
14:15:25.545 Error - Unknown HCI command: 8270 [0x204e] Length: 8
14:15:25.545 Parameters : 00 20 43 50 50 a0 00 01
14:15:25.545 RCVD [1] Event from HCI. Name: HCI_Command_Complete (Hex Code: 0x0e Param Len: 4)
14:15:25.545 Num HCI Cmd Packets : 1 (0x01)
14:15:25.545 Cmd Code : 0x204e (?? Unknown ??)
14:15:25.545 Error - Unknown HCI command: 8270 [0x204e]
What is command 0x204e? I can't seem to find any documentation on this command.
Solved! Go to Solution.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
0x204e is the LE Set Privacy Mode Comand. You can find the command details in the Core_v5.0 vol2, Part E, 7.8.77.
Or you can also find it in the CyBluetool CyBluetool (Windows Installer)

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
0x204e is the LE Set Privacy Mode Comand. You can find the command details in the Core_v5.0 vol2, Part E, 7.8.77.
Or you can also find it in the CyBluetool CyBluetool (Windows Installer)

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Thank you for answering my question, Owen. So, what is reporting the Set Privacy Command as "Unknown"? Is it the BTSpy/ClientControl software or the CYW20719 module?

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
The BT Spy capture the HCI command between the host and the controller, then try to analyse it. The "Unknown" is caused by the BTSpy software.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Thank you once again, Owen. I very much appreciate your prompt replies.