Hello,
I am using CYBT-413034-02 custom board. In wiced studio6.4 in makefile.mk of Hello_sensor
APP_PATCHES_AND_LIBS += FM25Q04_sflash.a is writtern. But while programming i am getting error as cannot find FM25Q04_sflash.a file?
Where can I find FM25Q04_sflash.a file?
when i comment this line APP_PATCHES_AND_LIBS += FM25Q04_sflash.a no error detects, but my module doesn't get detected.
I am just uploading the Hello_sensor code. Code uploads successfully. In Android app cysmart I can detect my module? Is the module not advertising?
According to the below link I have change the patches file also.
Platform and New Patch Files For 20719B1 in WICED 6.4.0.61 - KBA228518
Thank You?
Solved! Go to Solution.
Hi,
APP_PATCHES_AND_LIBS += FM25Q04_sflash.a - this is not needed to use CYBT-413034-02.
However please follow the KBA for consistent behavior of BT: Platform and New Patch Files For 20719B1 in WICED 6.4.0.61 - KBA228518
If the device is not getting detected, then please do recovery procedure : Press and hold Recovery -> press and release reset button -> release recovery button
Please check if HCI UART & PUART is coming correctly in device manager.
Also you may include the HCI UART com port number in make target as demo.beacon-CYBT_413034_EVAL download UART=COMxx
Regards,
Anjana
Hi,
APP_PATCHES_AND_LIBS += FM25Q04_sflash.a - this is not needed to use CYBT-413034-02.
However please follow the KBA for consistent behavior of BT: Platform and New Patch Files For 20719B1 in WICED 6.4.0.61 - KBA228518
If the device is not getting detected, then please do recovery procedure : Press and hold Recovery -> press and release reset button -> release recovery button
Please check if HCI UART & PUART is coming correctly in device manager.
Also you may include the HCI UART com port number in make target as demo.beacon-CYBT_413034_EVAL download UART=COMxx
Regards,
Anjana