Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

AmHa_650526
Level 2
Level 2

1. I am using CYBT-413034-EVAL.

2. I have tried programming CYBT-413034-02 present on CYBT-413034-EVAL. I powered up the board using external dc power supply of 3.3 V (by connecting to VDD and GND pins present on J3 connector). I did not connect the USB port of the eval board to the PC. I pushed all the switches of SW4 and SW5 to OFF position.

3. I connected TTL level signals of HCI UART (namely UART_RXD, UART_TXD, UART_CTS, UART_RTS present on header J1) to another board with RS232 transceiver present on it. The RS232 level signals were connected to the PC DB9 connector.

4. Please remember that I selected the following setting in WICED Module Programmer GUI 

CYBT-413034-02 for Module Name

UART Adapter Board for Programming Board

Baud rate as 115200 under DUT Serial Port Setting

CTS flow control is ticked under DUT Serial Port Setting

4. The log in 1.jpg shows this.

5. The log in 2.jpg shows after resetting and recovering the board.

Please help.  

0 Likes
1 Solution
SheetalJ
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi AmHa_650526​,

Can you try selecting your firmware file path as WICED-Studio-6.2\20719-B1_Bluetooth\build\test_project-CYBT_413034_EVAL-rom-ram-Wiced-release\test_project-CYBT_413034_EVAL-rom-ram-Wiced-release.hex?

Also, recover the board before you click on Program in Module Programmer.

View solution in original post

3 Replies
AmHa_650526
Level 2
Level 2

Also I want to let you know that I am selecting "Firmware File Path" in Wiced Moule Programmer as

"WICED-Studio-6.2\20719-B1_Bluetooth\build\test_project-CYBT_413034_EVAL-rom-ram-Wiced-release\test_project-CYBT_413034_EVAL-rom-ram-Wiced-release.ota.hex"

0 Likes
SheetalJ
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi AmHa_650526​,

Can you try selecting your firmware file path as WICED-Studio-6.2\20719-B1_Bluetooth\build\test_project-CYBT_413034_EVAL-rom-ram-Wiced-release\test_project-CYBT_413034_EVAL-rom-ram-Wiced-release.hex?

Also, recover the board before you click on Program in Module Programmer.

Thank you. I performed programming as advised by you and it succeeded.

Thanks for quick reply.

0 Likes