cancel
Showing results for 
Search instead for 
Did you mean: 

Studio Bluetooth

gusic_3800826
New Contributor

HI,

I am using the CYBT-413034-02 WICED capable BT module for which the underlying processor is CYW20719.

SDK ver is 6.2

WICED-SDK Version: Wiced_006.002.001.0002

I took a reference application for A2DP sink from 20706 packages and used the CYBT-413034 platform to build and program the module.

I was able to advertise and connect the "wiced a2dp sink" device to the host on a Windows 10 PC and an Android 9 Mobile phone. The BT module connected correctly and appears as an audio interface in the Windows 10 PC.

When I try to stream the audio to the BT module, I can't see the data out from the module on the configured I2S lines.

I2S I/O configs:

I2S_DI        P0

I2S_DO      P29

I2S_WS      P38

I2S_CLK    P10/P11

I tried to place a scope on the WS and CLK lines to see if I get I2S data bytes and the changing WS and Clock pulses. But it simply does not show anything.

After some search on the Cypress forums, I found that the current WICED Studio does not support I2S on CYW20719. Is it true?

Is there an option to import older projects/libraries and compile them for 20719 modules to get it working. The forums and associated links say that the user application cannot control the I2S peripheral directly, but is there any way I can test out the I2S interface using an existing working sample code for the 20719.

Thanks,

Gurpreet Singh

0 Likes
1 Solution
Owen_Zhang123
Moderator
Moderator

The 20719 doesn't support audio application. You may use 20706-based module or 20721. For each profile supported, please refer to the following blog: WICED Bluetooth Software Features

View solution in original post

4 Replies
Owen_Zhang123
Moderator
Moderator

The 20719 doesn't support audio application. You may use 20706-based module or 20721. For each profile supported, please refer to the following blog: WICED Bluetooth Software Features

gusic_3800826
New Contributor

Are there any plans to have A2DP Sink over I2S patch in the future SDK releases? If the support is planned in the coming 2-3 months, I can continue with 20719 for rest of the application.

0 Likes
Owen_Zhang123
Moderator
Moderator

The audio application will be supported with 20721. There is no plan to support audio on 20719.

0 Likes
MichaelF_56
Moderator
Moderator

Please reach out to your local Cypress sales/distribution team to discuss a CYW20721 engagement as this device and the associated SDK are not supported within the broad market.

0 Likes