Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello, we are developping a product based on module CYBT-353027.

It seems that modules we receive are programmed with a MAC address formatted the following way:  "20:70:6A:20:XX:XX".

This looks like the OUI part (Organisationally Unique Identifier) is set to  "20706", which looks lke the chipset familly embedded in the module 353027 module.

Looks like a temporary debug MaC address, not like an official one.

My question is the following:

- Can we use this MAC address in our final product or do we have to program a real MAC address on the module during our factory End Of Line process (MAC address that would be provided by Cypress in a SerailNumber-MAC address database/file) ?

Thank you for your help.

0 Likes
1 Solution
Owen_Zhang123
Moderator
Moderator
Moderator
5 questions asked 500 solutions authored 250 sign-ins

The module should be programmed with EZ-Serial and with a static random mac address. As the CYBT-353027 module is newly released, the ez-serial may not be programmed. The mac address "20:70:6A:20:XX:XX" is just for test in the factory. You need to programm a new mac address.

You can either apply a new mac address in the IEEE website or just use a static random mac address.

View solution in original post

1 Reply
Owen_Zhang123
Moderator
Moderator
Moderator
5 questions asked 500 solutions authored 250 sign-ins

The module should be programmed with EZ-Serial and with a static random mac address. As the CYBT-353027 module is newly released, the ez-serial may not be programmed. The mac address "20:70:6A:20:XX:XX" is just for test in the factory. You need to programm a new mac address.

You can either apply a new mac address in the IEEE website or just use a static random mac address.