Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

AkMu_1694496
Level 1
Level 1
First like given

Dears,

Our customer would like to try to evaluate CYBT-353027-02 for their handy gas sensor equipment.

They have already had CYBT-353027-EVAL for the evaluation.

1) Can customer use CYBT-353027-EVAL in Japan ?

Actually customer could not find MIC certification mark at the EVB.

On the other hand CYBT-353027-02 has already been certified conformance to technical standards that number is 203-JN0859.

2) How to get the labeling of MIC for customer Production ?

In case of customer production, it is needed to identify the certification mark on the module or final products.

How our end customer get the certification label ?

It would be appreciated if someone advise the above two inquiries.

Best regards

0 Likes
1 Solution
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hi,

The KBA (RF Regulatory Certifications for CYBT-353027-02 EZ-BT™ Module - KBA223952)  is right and CYBT-353027-02 is MIC certified.

The active datasheet in system is still preliminary version, it will be updated this week with the MIC certified value.

MIC log and ID are on module for MP (Mass production ) boards, but they are not shown for NPI boards.

Thanks & regards

Anjana

View solution in original post

5 Replies
BoonT_56
Employee
Employee
500 likes received 250 likes received 100 likes received

I quote pg40 of the datasheet in here:

MIC Japan

CYBT-353027-02 is certified as a module with certification number TBD. End products that integrate CYBT-353027-02 do not need

additional MIC Japan certification for the end product. End product can display the certification label of the embedded module.

Is the above helpful?

0 Likes
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hi,

The KBA (RF Regulatory Certifications for CYBT-353027-02 EZ-BT™ Module - KBA223952)  is right and CYBT-353027-02 is MIC certified.

The active datasheet in system is still preliminary version, it will be updated this week with the MIC certified value.

MIC log and ID are on module for MP (Mass production ) boards, but they are not shown for NPI boards.

Thanks & regards

Anjana

Hi Anjana

Thank you so much for your reply and well noted that CYBT-353027-02 have been certified each regulation.

We would like to know especially as following two points.

1) Our customer can evaluate CYBT-353027-02 using CYBT-353027-EVAL even CYBT-353027-EVAL does not show MIC mark on the board or Module, right ?

2) Regarding your reply "MIC log and ID are on module for MP (Mass production ) boards, but they are not shown for NPI boards.",

do you mean that can customer see the MIC LOGO and ID on top of module visibility ?

Best regards

Akira

0 Likes

Hi Akira San,

1) Yes you can

2) Yes. Please refer to the attached image.

Thanks,
Anjana

Hi Anjana

Thank you soooo much !!

It is perfect !

Regards

Akira

0 Likes