Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

YoJa_3107936
Level 5
Level 5
50 sign-ins First like given 100 replies posted

Hi

Please tell me the initial state, when it was shipped.

(Transmission level, BER, frequency deviation)

Thanks

Y.Jiang

0 Likes
1 Solution
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

The initial Tx power will depends on which you have set and programmed to the chip. The Tx parameter can be set in the application run time.

By default CYBT-343026-01 is shipped with Ez-serial FW . And the default Tx power set in that is 0dB (http://www.cypress.com/documentation/software-and-drivers/ez-serial-ez-ble-module-firmware-platform)

RF test reports and Certificates of CYBT-343026-01 is available here: https://community.cypress.com/docs/DOC-14196

Thanks & Regards,

Anjana

View solution in original post

1 Reply
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

The initial Tx power will depends on which you have set and programmed to the chip. The Tx parameter can be set in the application run time.

By default CYBT-343026-01 is shipped with Ez-serial FW . And the default Tx power set in that is 0dB (http://www.cypress.com/documentation/software-and-drivers/ez-serial-ez-ble-module-firmware-platform)

RF test reports and Certificates of CYBT-343026-01 is available here: https://community.cypress.com/docs/DOC-14196

Thanks & Regards,

Anjana

This widget could not be displayed.