CYBT 343026: Recovery operation

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
YoJa_3107936
Level 5
Level 5
Distributor - Macnica (Japan)
100 sign-ins 50 sign-ins First like given

Dear everyone

Could you answer the below questions ASAP?

1, Is the mbt tool executed in recovery mode operation?

2, When doing with the hand during the recovery operation,

    how many seconds is Max to press the recovery button and the reset button

3, How to check the state of FW, Confirm whether it is broken

Have a good day.

Thanks

Y.Jiang

0 Likes
1 Solution
lock attach
Attachments are accessible only for community members.
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hi,

1) Is the mbt tool executed in recovery mode operation?

A) No, the device should not be in recovery mode for mbt tool to work. Please go through the attached doc for steps.

2) When doing with the hand during the recovery operation,

    how many seconds is Max to press the recovery button and the reset button

A) There is no maximum time constraints. The normal recovery procedure which needs minimum timings is as below:

  • Press and hold the Recovery button (SW3).
  • Press and hold the Reset (SW2) button for 1 second.
  • Release SW2
  • Release SW3.

3) How to check the state of FW, Confirm whether it is broken

A) Recovery procedure is used during device programming stage. Recovery procedure is to reset a WICED evaluation board to factory defaults if it has become unresponsive to WICED Studio download attempts. This will reset the board to reboot to the default state, ready to accept a new download. This can be necessary if a previous application had set the UART to an unrecognized baud rate (115200 and 3000000 are the default baud rates attempted by the download process), or if the serial flash had been corrupted.

Thanks & Regards,

Anjana

View solution in original post

0 Likes
3 Replies
lock attach
Attachments are accessible only for community members.
AnjanaM_61
Moderator
Moderator
Moderator
10 questions asked 5 comments on KBA First comment on KBA

Hi,

1) Is the mbt tool executed in recovery mode operation?

A) No, the device should not be in recovery mode for mbt tool to work. Please go through the attached doc for steps.

2) When doing with the hand during the recovery operation,

    how many seconds is Max to press the recovery button and the reset button

A) There is no maximum time constraints. The normal recovery procedure which needs minimum timings is as below:

  • Press and hold the Recovery button (SW3).
  • Press and hold the Reset (SW2) button for 1 second.
  • Release SW2
  • Release SW3.

3) How to check the state of FW, Confirm whether it is broken

A) Recovery procedure is used during device programming stage. Recovery procedure is to reset a WICED evaluation board to factory defaults if it has become unresponsive to WICED Studio download attempts. This will reset the board to reboot to the default state, ready to accept a new download. This can be necessary if a previous application had set the UART to an unrecognized baud rate (115200 and 3000000 are the default baud rates attempted by the download process), or if the serial flash had been corrupted.

Thanks & Regards,

Anjana

0 Likes
YoJa_3107936
Level 5
Level 5
Distributor - Macnica (Japan)
100 sign-ins 50 sign-ins First like given

Thank you for your cooperation.

About 3)

So  I  think that we can't confirm from the LED on the board whether the FW is a problem, is it correct?

Thanks

Y.Jiang

0 Likes

Hi,

Q) So  I  think that we can't confirm from the LED on the board whether the FW is a problem, is it correct?

A) Yes, you can't

Thanks,
Anjana

0 Likes