CYBT-343026-EVAL: how to use WICED_BT_TRACE outputs for debug purposes?
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
Greetings,

What must I do in order to be able to visualize the WICED_BT_TRACE output messages with the CYBT-343026-EVAL so that I can debug my application?

What I have made so far is opening the COM port that corresponds to the HCI_UART in tera term at a baudrate of 115200 (the same as I set in the application I am testing).

However, all I get to see is a bunch of unanderstandable data and some chunks of the SDP Database, like the SDP_ATTR_SERVICE_NAME.

I attatch a capture of what is displayed in tera termwhenever I connect to the module from my phone.

Thanks in advance for your help.

Regards.

0 Likes
1 Solution
LJYe_2922526
Level 5
Level 5
25 likes received 10 likes received 5 likes given

Try opening PUART. HCI UART is normally used for WICED HCI control messages.

Alternatively call wiced_set_debug_uart() to change where debug traces are routed.

If you run the demo client_control program, use BTSpy to look at debug traces.

Good luck!

View solution in original post

2 Replies
LJYe_2922526
Level 5
Level 5
25 likes received 10 likes received 5 likes given

Try opening PUART. HCI UART is normally used for WICED HCI control messages.

Alternatively call wiced_set_debug_uart() to change where debug traces are routed.

If you run the demo client_control program, use BTSpy to look at debug traces.

Good luck!

Anonymous
Not applicable

That works just fine.

Thank you very much!

Best regards.

0 Likes