CYBT-343026-01 GPIO06 not working as input pin.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
NeDh_4602711
Level 5
Level 5
5 solutions authored First solution authored 50 replies posted

Hello,

I am using WICED Studio 6.2 with CYBT-343026-01 and I am using GPIO06 pin for reading input with pullup as the default state. But When I trying to check the status of GPIO06 it shows 0 continuously. it should be 1 when the button is not pressed. and I am expecting it should be 0 only If the button is pressed. Also, I have checked with GPIO 3 pin and it works perfectly.

Is there any limitation that I cannot use this GPIO6 pin as input?

Thanks and regards,

Neeraj

0 Likes
1 Solution
NeDh_4602711
Level 5
Level 5
5 solutions authored First solution authored 50 replies posted

Hi,

Instead of GPIO06 I have used P11 in function and it works for me.

Regards,

Neeraj Dhekale

View solution in original post

1 Reply
NeDh_4602711
Level 5
Level 5
5 solutions authored First solution authored 50 replies posted

Hi,

Instead of GPIO06 I have used P11 in function and it works for me.

Regards,

Neeraj Dhekale