Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Studio Bluetooth Forum Discussions

TaMi_1708256
Level 2
First like given 25 sign-ins 10 replies posted
Level 2

Hi

Could you tell me the "Drive capability"(xx mA) of each PIN on CYBT-343026-01 module when it is set to output ?

Regards,

T.M.

0 Likes
1 Solution
BoonT_56
Employee
500 likes received 250 likes received 100 likes received
Employee

The GPIO are capable of driving up to 8 mA at 3.3 V or 4 mA at 1.8 V. However for P26, P27, P28, and P29, they are capable of driving up to 16 mA at 3.3 V.

View solution in original post

4 Replies
BoonT_56
Employee
500 likes received 250 likes received 100 likes received
Employee

The GPIO are capable of driving up to 8 mA at 3.3 V or 4 mA at 1.8 V. However for P26, P27, P28, and P29, they are capable of driving up to 16 mA at 3.3 V.

TaMi_1708256
Level 2
First like given 25 sign-ins 10 replies posted
Level 2

Hi

Thank you

In addition.

Is this same (8 mA at 3.3V) in the following the "special" PINs ?

PAD 6  SPI2_CS_N

PAD 9  SPI2_MOSI

PAD 16 UART_TXD

PAD 18 UART_RTS

Thanks

T.M.

0 Likes
BoonT_56
Employee
500 likes received 250 likes received 100 likes received
Employee

Usually we do not talk about electrical current levels for digital communications like UART. But I noted that for digital IO, the max output current at 3.3V is 4mA (Table12 of CYW20706 datasheet). You may want to download a copy of the 20706 datasheet for more information on this chip.

TaMi_1708256
Level 2
First like given 25 sign-ins 10 replies posted
Level 2

Hi

I understood it.

Thanks

0 Likes