[CYBT-343026-01] All Pin state during reset

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
TaMi_1708256
Level 2
Level 2
50 sign-ins First like given 25 sign-ins

Hi

Please let me know the state of the "ALL PINS" during reset?

I know what UART pins was discussed below.

[CYBT-343026-01] Pin state during reset

I would like to know similar information about following.

1pin    P0_P34

2pin     I2C_SCL

4pin     I2C_SDA

5pin     P2_P37_P28

6pin     SPI2_CS_N

8pin     SPI2_MISO

9pin     SPI2_MOSI

10pin    SPI2_CLK

11pin    GPIO_0

12pin    GPIO_1

14pin     GPIO_4

15pin     P4/P24

19pin     GPIO_7

22pin     GPIO_3

23pin     GPIO_6

Thanks

TM

0 Likes
1 Solution
SheetalJ
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 500 likes received

Hi mizukosi_1708256,

'During' reset, all pins will be in Hi-z state only. Just after reset, pins will behave as per the defined state in registers or application(if already programmed).

View solution in original post

2 Replies
SheetalJ
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 500 likes received

Hi mizukosi_1708256,

'During' reset, all pins will be in Hi-z state only. Just after reset, pins will behave as per the defined state in registers or application(if already programmed).

Hi SheetalJ_96

Thank you for your reply.

I got it.

Thanks

TM

0 Likes