Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

YoJa_3107936
Level 5
Level 5
50 sign-ins First like given 100 replies posted

Hi

I would like to confirm the following information.

1. Can I use mbt.exe without installing WICED-Studio-6.x to  test and verify the RF performance?

I think it can be used basically , but are there any precautions?

2. When performing Radio TX Test item, Class1 test using MBT, is tx_power the maximum value +3dBm?

>tx_power: –25 dBm to +3 dBm

MBT tool and CyBluetool tool can also test and verify the RF performance, which one do you recommend?

Thanks,

Yang

1 Solution
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hello YoJa_3107936 ,

1. yes you can use mbt.exe without installing SDK. If you already have it.

2. Yes correct

MBT tool and CyBluetool tool can also test and verify the RF performance, which one do you recommend?

- Both use the same HCI commands . One is command line and one is GUI. You may use which ever is comfortable.

Regards,

Anjana

View solution in original post

0 Likes
1 Reply
AnjanaM_61
Moderator
Moderator
Moderator
First comment on KBA 5 questions asked First question asked

Hello YoJa_3107936 ,

1. yes you can use mbt.exe without installing SDK. If you already have it.

2. Yes correct

MBT tool and CyBluetool tool can also test and verify the RF performance, which one do you recommend?

- Both use the same HCI commands . One is command line and one is GUI. You may use which ever is comfortable.

Regards,

Anjana

0 Likes