I was wondering if it was possible to remove the reliance of client control for the watch demo (such that it can connect MAC addresses hard coded into the demo). I am struggling to get it to work without opening the COM port using client control.
Is there a setting that disables functionality unless it is connected via Client Control? If so how can i disable it?
Solved! Go to Solution.
Hi MaCh_4826131,
I don't think there is any way to disable ClientControl functionalities. If you do not want to use any of the functionalities, you can remove those particular libraries and implementation from the code example.
Let me know if I understood and answered the question correctly.