Hi,
请先阅读Audio_Heaset这个Demo的Readme.md,它会给你一些提示,链接在下方:
https://github.com/Infineon/mtb-example-btsdk-audio-headset
其中有一些提示可能会引起你的注意:
This application can run as a standalone Headset or in association with ClientControl. When running in standalone mode, it is required that the 20706 controls the codec chip. Currently this is not implemented.
To use this in stand alone mode:
- Ensure that the STANDALONE_HEADSET_APP flag is enabled.
- The User button is configured to demonstrate multiple functionality.
- The button has 2 states, short press and long press. Both of them have certain features configured.
- Button Short Press Cases:
- Play/Pause music streaming.
- Accept/End incoming call/ongoing call.
- End an outgoing call.
- Button Long Press Cases:
- Last number redialing when in IDLE state.
- Reject an incoming call.
- Put an existing call on hold.
Best regards