Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Speed (Magnetic sensor) Forum Discussions

Sort by:
AdamR
Speed (Magnetic sensor)
Hi there,Is there a programming kit available for programming of the TLE4959x EEPROM? I would like to evaluate them and I was wondering if such a kit ... Show More
Sayali234
Speed (Magnetic sensor)
Hello Team,     Please suggest a latch-type hall sensor that withstands lower temperature rating up to -55C. The package is not a concern yet. Below a... Show More
suyihua
Speed (Magnetic sensor)

What is the corresponding model of 46C33P?

WuXiaoyun
Speed (Magnetic sensor)
Hello, the Rm given in the TLE5041plusC datasheet is 30Ω-75Ω, is this the corresponding value in the case of a supply voltage of 4.5V? If the power su... Show More
rsiigod
Speed (Magnetic sensor)
Hi everyoneGood day~ I don't know the differences between TLE5028C-XAI & TLE5028C-XAA from the datasheet. The following is my opinion, I don't know if... Show More
Forum Information

Speed (Magnetic sensor)

In this forum you can post your questions, comments and feedback about the XENSIV™ Speed sensors. This sensor family is based on integrated Magneto Resistive (ixMR) or hall-based technologies in order to determine linear and rotational speed. Our Speed sensors can be used with ferromagnetic gear tooth wheels or encoders to measure speed and position and they are essential components for the function of safety and powertrain applications like rotating shafts. Here you can also find the links to the latest board pages, documents and FAQs.