Speed (Magnetic sensor) Forum Discussions
Hi there,
Is there a programming kit available for programming of the TLE4959x EEPROM? I would like to evaluate them and I was wondering if such a kit was available. If not, is there a recommended programming circuit I could build to test them with?
Thanks,
Adam
Hello Team,
Please suggest a latch-type hall sensor that withstands lower temperature rating up to -55C. The package is not a concern yet. Below are details of the hall sensor specifications. This we required for Aerospace and defense application
Voltage – 2.7V to 5V/24V
Output type – Open drain/open collector
Technology – Hall effect
Type - Latch
Polarization – South /North
Package – Any
Temperature - -55 °C to greater than +125 °C
Regards,
Sayali Shinde
Show Less
Hello, the Rm given in the TLE5041plusC datasheet is 30Ω-75Ω, is this the corresponding value in the case of a supply voltage of 4.5V? If the power supply voltage is set to 15V and the Rm is 470Ω, will there be any problems when using the IC?
Or what is the minimum and maximum value of Rm when the supply voltage is 15V?
Hi everyone
Good day~
I don't know the differences between TLE5028C-XAI & TLE5028C-XAA from the datasheet.
The following is my opinion, I don't know if it is correct:
TLE5028C-XAI-D28 CW 90us, CCW 45us
TLE5028C-XAA-D28 CW 45us, CCW 90us
Or is there a better description different from the datasheet?
Best Regards
Rsiigod