Recent discussions
I use eprom flash memory CAT24C64 with I2C channel for CY8C4146AZI-S423 chip, PSoC Creator 4.4. I made a short test project, it works well, but if I run this project in debug mode even without breakpoints, the MemoryWrite and MemoryRead APIs return DEVICE_BUSY instead of SUCCESS. For this reason, I cannot debug a more complex project where I use this flash. I tried to set CyDelay with different times after these APIs, useless for debug mode, but once this project is programmed it works well with CyDelay(10). Maybe I'm missing something?
Show LessI am looking for documentation on the CY7C024BVF-15AXI, but cannot find any documentation on what "BVF" indicates in the part number.
I can find documentation on the CY7C024AV-15AXI, and CY7C024BV-15AXI, but nothing on the CY024BVF-15AXI.
There is however a note on page one of the CY7C024AV datasheet Rev J (#38-06052 Rev *J) that "AV" parts are functionally equivalent to "BV" parts, but no mention of "BVF".
Thank you for your help.
Hello everyone!
I'm looking to program the CY7C287. Would anyone be able to point me in the right direction?
Thank you for any help you can give!
Show LessCY7C024AV is a FIFO. What is the response time versus temperature performance? Specifically, will the device be slower at lower temperatures?
We have been a user of F-RAM part FM25V02A for about 8 years. We recently have had instances where some of the data locations appear to getting cleared.
We are looking at the system electrical and software behavior but I wanted to reach out to see if there are any known production issues with this part in the recent past that could help explain our issue.
Show LessI need documentation regarding CYRS1069G30-12GGMB. I am designing the PCB!
Our needs are very urgent!
Thank you
We are using S40410081B1B2W00 in our board.
The voltage is supplied 3.3V. But in software we are unable to detect the EMMC - S40410081B1B2W00 .
We have checked the voltage rail, looks fine.
The RESET pin also High. Please support us in debugging.
Show Less
Hi Tech,
Per customer's request, could you help check and share with us PDN ( product discontinued notice ) for EOL part#CY7C4285V-15ASI? What's the alternative part?
Thanks.
Show LessHello,
Could you provide the Thermal Resistance Theta Jc[℃/W] and Tj[℃] of HOTLink II devices?
MPN: CYP15G0101DXB-BBXI
I can't find it out in datasheet.
https://www.cypress.com/file/113721/download
Best Regards,
Naoaki Morimoto
Show LessHi Cypress
We need a Cypress memory (pin to pin and same operation voltage) for replace EVERSPIN/MR25H256CDF , Can you suggest a Cypress component for it , Thank!!
Show Less