Recent discussions
I am working on a design which uses a CPLD to control two CYF0018V FIFOs ,what would be ideal would be a behavioural HDL model of the FIFO but in the absence of these I am looking for a timing diagram showing burst rea/write cycles on these devices.The datasheet mentions the fact that they support burst read/writes but I cannot find any further information.
Thanks
Show LessHi,
I am intefacing MPC8641D to CY7C0833AV DPRAM memory using GPCM mode in PowerPC.
I was able to perform Read/Write transactions to the DPRAM.
Now I need to do burst read from DPRAM using UPM mode in PowerPC.
Does the DPRAM (Part No:CY7C0833AV/Density 9-Mbit) supports the burst read/write operation?
Regards
SID
Show LessCan anyone tell me what the internal (physical) configuration of the C7C09389 is?
The external interface is 64K x 18 but I imagine that the internal memory array is probably something more 'square'.
We have had a very rare failure in one of our systems that is hard to recreate, and I am trying to determine if we might be occastionally violating some internal boundary condition. The error has a pattern to it, and this may give me a clue as to the cause.
Thanks!
Show LessCypress now offers self-paced tutorials on FIFOs. These training modules start out with the fundamentals of FIFO operation and later introduce the special features of these devices and their applications. These tutorials are ideal for beginners as well as for advanced users.
These web-based tutorials can be found in the "Training On-Demand" section of our website:
Asynchronous FIFOs: http://www.cypress.com/?rID=53985
Synchronous FIFOs: www.cypress.com/
Please provide your feedback on these tutorials as it will help us improve the content and quality of the modules.
Thanks!
Show LessHi,
Cypress has recently enhanced the Training Module contents on its website. Please check the following link, for a training module on basics of Synchronous Dual-Port RAM's.
http://www.cypress.com/?rID=12642
Please take these modules at your convenience and let us know your feedback.
Thanks!
Show Less- « Previous
- Next »