Specialty Memory Forum Discussions
Hello,
Could you provide the Thermal Resistance Theta Jc[℃/W] and Tj[℃] of HOTLink II devices?
MPN: CYP15G0101DXB-BBXI
I can't find it out in datasheet.
https://www.cypress.com/file/113721/download
Best Regards,
Naoaki Morimoto
Show LessHi Cypress
We need a Cypress memory (pin to pin and same operation voltage) for replace EVERSPIN/MR25H256CDF , Can you suggest a Cypress component for it , Thank!!
Show LessHello All,
I Am facing issue with CY7C1645KV18 Verilog model simulation with Xilinx MIG generated Test bench. Getting Calibration complete not done error. If anybody facing the issues with Verilog model simulation on this part or any other part?. If yes please suggest the workaround for solving this issue.
Thanks With Regards,
Venkatesh Babu.N
India.
Show LessHello,
About AgigA Tech's AGIGA9824-103JCB
What types of NVDIMMs does this product support?
Also, please tell me the manufacturer and model number of the NVDIMM with a opertion confirmation.
Best regards,
Naoaki Morimoto
Show LessHello All!
first time came on this forum,
need help about programming the following ICs:
- Cypress 7C245A, DIP
- Cypress 7C281A, DIP
- Cypress 7C282A, DIP
- Cypress 7C287, DIP
- Cypress 7C335, DIP & PLCC 28 pin
using which programmer, they can be programmed?
Anticipating your kind response,
Thanking you in advance,
With Regards,
Dev Raj
Show LessAs the attached case reply, the design for QDR4 with Xilinx Kintex Ultrascale could be reviewd.
we have nearly finished that design, how can I send the schematic to Mr/Mrs Pradipta for review?
Show Lesswe are using QDR IV:Cy7c4142kv13, connect to Xilinx ultrascale fpga, is there any reference design include schematic,pcb, and qdriv controller fpga design?
for no such detail information attached in AN84060:QDR®-IV Design Guide.
also,could the schematic lib of Cy7c4142kv13 or the pin definition list in excel be provided?
Show Lesshello, I bought 2 AM29F010B. I need to connect them to a port from MCU (AVR) with any latch or multiplex IC.
Could you help me telling me which IC can I use to communicate 2 AM29F010B with one MCU? Thank you
Show LessHello for a new design what is the replacement components for CY7C43683AV or what is the components with the closest features and performances. The pinout interface can be différent.
Best regards
Show Less