Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

ShFu_1540346
Level 4
Level 4
25 replies posted 10 replies posted 10 questions asked

Dear all,

The customer is now using IDT's 7025PF and we are trying to replace it with Cypress DPRAM.

The customer's board now works on 5.0V, but they are changing it to 3.0V.

Based on the requirements below,  is it correct to suggest CY7C025AV-25AXI?

IDT

part number=7025PF

voltage=3.0V

8K*16

Industrial grade

TQFP 100

Pin compatible and timing compatible with 7025PF

Thank you,

Shun Furusawa

1 Solution
Anonymous
Not applicable

Hello Furusawa San,

The speed of Cypress device is 25ns, I hope the speed of IDT is also 25ns. Both are pin compatible.

Yes CY7C025AV-25AXI looks the closest replacement for IDT part.

Thanks,

Krishna.

View solution in original post

2 Replies
Anonymous
Not applicable

Hello Furusawa San,

The speed of Cypress device is 25ns, I hope the speed of IDT is also 25ns. Both are pin compatible.

Yes CY7C025AV-25AXI looks the closest replacement for IDT part.

Thanks,

Krishna.

ShFu_1540346
Level 4
Level 4
25 replies posted 10 replies posted 10 questions asked

Hi Krishna-san,

Thank you for your comment.

I will check about the speed.

Thank you,

Shun Furusawa

0 Likes