Software Forum Discussions
Browse the Community
ModusToolbox™
The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.
DAVE™
PSoC™ Creator & Designer
Discussion forum regarding PSoC Creator & Designer Software topics.
Wi-Fi Bluetooth for Linux
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).
Featured Discussions
v5.15.58-2023_0901
Release Date
2023-09-01
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
* Backports package (cypress-backports-v5.15.58-2023_0901-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.15.58-2023_0901.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.15.58-2023_0901.tar.gz)
* Device tree files (cypress-devicetree-2023-09-01.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_10-2023_0901.tar.gz)
* Cypress customer patch (cypress-custom-patch-5.4.21.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Checksum
sha256sum:
98d7527606017f851fccb91ef557efaf778c5b2b48264942ed0ea9d7c0a1516a cypress-fmac-v5.15.58-2023_0901.zip
7f88760a74174713d4ffd7aec3479f592c5fa9f876c92941662897454a5feb53 cypress-backports-v5.15.58-2023_0901-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
1a792aa55d847917a7a741418493427ff30dfff10eacf9218b58f192c570942c cypress-custom-patch-5.4.21.tar.gz
1fe05a168cb6e3697e1a7610760f8e86393f53f8fc22b47645b6d00f59365e6d cypress-devicetree-2023-09-01.tar.gz
f0b9d3b25a71b4de69593f511d7e99b49dae8528eb9797983f89f584294963c1 cypress-firmware-v5.15.58-2023_0901.tar.gz
ad057de3baa941ddf59af8b784fe3c3ff1173fe5e04146f07db85362e2d8bb7b cypress-hostap_2_10-2023_0901.tar.gz
96911757cd613afb743db1c504fc3db2184456f3af0d79a814e6463ce384689a cypress-patch-v5.15.58-2023_0901.tar.gz
2023-09-11 Initial Post
- Add 43455 FW
hi,
what is the syntax of the files mtbgetlibs use?
due to issues with github we want to mirror all infineon repositories locally, but we don't expose our internal git server over https - thus we need to use ssh references. what is the correct syntax of the mtb files for git-over-ssh repositories?
thanks, jacob
Show LessRequest for iAP2 SDK for the latest Modus 3.1 and BTSDK 4.x.x. About Apple MFi license information is,
-Company Name : Aroot.co.,Ltd. ,korea
Show Less
Hi
DAVE App "EVENT_GENERATOR" for ERU has only single "pattern" and no "tout" output.
According to the reference manual, OGU in ERU has 4 signals to detect pattern, and "ERU_TOUT" without gating.
Would you tell me the description of RM is correct and the DAVE App is not corret ? Dave App
Reference Manual
Best Regards,
Hayashi.K
Hi All,
In an effort to simplify the user journey, we have merged all old forums under the ModusToolbox™ category (namely - PSoC™ 6 SDK, Bluetooth SDK, AWS IoT SDK, Mbed SDK, Any cloud SDK and ModusToolbox™ General) to this new ModusToolbox™ forum. So, you will not have to navigate beyond level 3 in the menu anymore, to ask or look up your ModusToolbox™ related queries... saving you some time, every time.
Old Navigation Journey
New Navigation Journey
All the topics you have been following in the old ModusToolbox™ category is now present in the new ModusToolbox™ forum. If you have bookmarked a particular forum, it will get automatically redirected to this new one, as well as any threads under it.
Hope you like the new experience.
Please let us know for any queries.
Regards,
Sharit
Infineon Developer Community team
Tip: If Modus Shell 1.4.0 is unresponsive, try accessing it by clicking on the Terminal tab within Eclipse for MTB and retarting Eclipse for MTB.
This may be something I implemented incorrectly
- or - This could be a helpful tip for anyone who finds Modus Shell 1.4.0 unresponsive.
Upon my first attempt to use Modus Shell 1.4.0 from the Windows Start Menu, after installing ModusToolbox 3.1, the application would NOT produce a prompt.
Modus Shell 1.3.1 and Modus Shell 1.3.0 both quickly produce a path and prompt to accept user input.
I was able to access Modus Shell through Eclipse IDE for MTB 3.1.
After closing then restarting Eclipse for MTB, Modus Shell 1.4.0 now works fine.
Note: Eclipse was open when I was trying to start Modus Shell from Windows directly. After restarting Eclipse, I am able to open Modus Shell 1.4.0 while Eclipse is open.
Greg
Show Less
The latest linux driver and software can be accessed here:
Wi-Fi Driver source package: https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Cypress-Linux-WiFi-Driver-Release-FMAC-2023-09-01/td-p/492862
Github link: https://github.com/Infineon/ifx-wireless-drivers/tree/RTM/v5.15.58-godzilla
The older/archived Wi-Fi driver releases can be accessed here:
Show LessProvided as a collection of development tools, libraries, and embedded run-time assets, ModusToolbox™ Software is architected to provide a flexible and comprehensive development experience.
Run-time software includes of middleware, device drivers, and code examples, and are regularly updated to include new features, minor bug fixes, and other enhancements. Updated software repositories may by published asynchronously or are otherwise rolled into a quarterly release cycle, with updated release notes and documentation, covering updates made throughout the previous quarter.
Latest features included in the June 2023 Quarterly release of run-time software
- Machine Learning middleware library v2.0.1
- The ModusToolbox™ ML Middleware Library is a set of helper functions to handle the Machine Learning models and capability to receive stream validation data.
- v2.0.1 includes functions enabling proper quantization of data:
- mtb_ml_utils_model_quantize()
- mtb_ml_utils_model_quantize()
- Class B libraries and code examples for PSoC™ 4
- Essential set of examples, libraries, and documentation demonstrating how to perform MCU functionality tests using the Class-B Self-Test Libraries (STL) on PSoC™ 4 devices
- PSoC™ 4 Class B Package available from the Infineon Developer Center
- Additional middleware for XMC7000
- Support for Bootloader capabilities based on MCUBoot
- Support for image signing via CySecureTools
- Connectivity middleware support (MQTT, HTTP Client / Server) enabled via the Ethernet Core FreeRTOS lwIP mbedTLS library
- New Code Examples
- Wi-Fi HTTPS Client: demonstrating an implementation of an HTTPS client with PSoC™ 6 MCU and AIROC™ CYW43xxx Wi-Fi & Bluetooth® combo chips
- Bluetooth A2DP Source: demonstrating streaming audio via Bluetooth Classic A2DP source profile from PSoC™ 6 to external Bluetooth speaker/earbuds)
- FreeRTOS-POSIX: demonstrating the usage of FreeRTOS-POSIX library for Infineon MCUs
- Updated Code Examples
- Multiple BTStack code examples have been updated to support CY8CEVAL-062S2-LAI-43439M2 and CY8CPROTO-062S2-43439 development boards
- Multiple BTStack code examples have been updated to support CY8CEVAL-062S2-LAI-43439M2 and CY8CPROTO-062S2-43439 development boards
- Segger emWin / AppWizard update
- Segger emWin library updated to v6.32
- Segger AppWizard updated to 1.38, available from the Infineon Developer Center
- Updated ModusToolbox™ Getting Started training module to include key features available within the latest ModusToolbox v3.1 tools release, including:
- New ModusToolbox™ Dashboard tool
- Integration of BSP Assistant with Project Creator and Library Manager
- Ability to create a BSP by specifying the chips used on the board (chip flow)
- Control of COMPONENTS and DEFINES in BSP Assistant
- Ability to rename BSPs during application creation
- Ability to store/manage/use local content for offline operation
- New SKIP_CODE_GEN variable to prevent automatic source code generation
- New troubleshooting section for common build errors
- New User Guides for VS Code, IAR, and µVision (in addition to Eclipse)
- Selectable programmer/debugger options
For additional details refer to:
Show Less
ModusToolbox™ 3.1 is now available for download from the Infineon Developer Center. This release includes several new features targeted at enhancing the ModusToolbox™ development journey from ‘Getting Started’ to ‘Final Hardware’. Below is a summary of the latest features included in this release, more details are available within the Release Notes.
New Features:
- A new dashboard application that serves as a central getting start utility, with easy access to key documentation, training modules, video tutorials, and relevant developer community forums. This dashboard application also provided guidance on creating a new ModusToolbox application for any of the supported IDEs, including Microsoft Visual Studio Code, IAR Embedded Workbench, Arm MDK (µVision IDE), or the included Eclipse IDE.
- Offline access for non-persistent internet connection is now addressed using the ModusToolbox™ Local Content Storage (LCS) Manager. This command-line utility can be used to generate a local copy of relevant content and online assets.
- BSP Assistant has been updated with an improved user interface and can be launched directly additional tools like Project Creator, Library Manager, and the Dashboard.
- BSP Assistant now provide a workflow for creating a new board support package (BSP) based on the selection of the target device (marketing part number) in additional to deriving from an existing BSP.
- The default toolchain configured within ModusToolbox v3.1 has been updated to Arm GNU Toolchain 11.3.rel1
- ModusToolbox™ v3.1 is supported on:
- Windows 7SP1, 10, 11
- macOS Catalina, Big Sur, Monterey
- Ubuntu 18.04 LTS, 20.04 LTS, 22.04 LTS
Key links:
- ModusToolbox™ Software overview
- Download (Window/Linux/macOS) from Infineon Developer Center
- Installation Guide
- User Guide
- Release Notes
Package Version
ahd-2023_0525
Release Date
2023-05-25
Description
Infineon Android release for the broad market.
This release has been qualified on IMX8 SDIO platform running Android 13.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Infineon's connectivity parts.
The release package includes:
* ahd
* AHDBinaries
* confs
* device
*imx8
* firmware
* hostapd_supplicant_src
* nvram
* 55572_AndroidBringup.pdf
* Android13_Godzilla_55572_SDIO_Release_Notes.pdf
* Infineon_55572_Wi-Fi_6_6E_User_Guide.pdf
Test Environment:
* IMX8 SDIO setup
* 55572 Sanity, 6G and 11ax features
Show Less