Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Software Forum Discussions

Browse the Community

ModusToolbox™

The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.

5913984 1198

WICED™ Studio

Discussion forum regarding WICED™ Studio related topics.

35162826 8508

AURIX™ Development Studio

The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).

133983 95

Recent discussions

Sort by:
ricardoquesada
PSoC™ 6 SDK
Hi, TL;DR: How to know the Interrupt number that is triggered when Counter triggers a Compare or TC ?   I'm migrating a project from PSoC Creator (Sch... Show More
WaMa_286156
PSoC™ Creator & Designer
Rolf Nooteboom helped develop a technique for writing and compiling firmware for PSOC5 on Linux and Macintosh (and Windows).  The overall system uses ... Show More
WS
AURIX™ Development Studio
Hi All, it seems that there is not any category for TC356/TC357 project on AURIX™ Development Studio (Version: 1.7.2) so, I want to know when AURIX™ ... Show More
Grama
ModusToolbox™ General
Hello New to Modus and stepping thru training. Working on the PWM to GPIO lab. I get an error othat it cannot find the Cy_TCPWM_MyPwm_Init funtion. Wh... Show More
jesubalan
Wi-Fi Combo
Hi ,   I am getting the below issue when I updated the MFG Test Application in Murata board. I haved updated the external flash with respective APPS.b... Show More
The_Novice
CIRRENT™ Product Analytics
Hello, I hope this is the right forum/place to ask my question. I need some help and hand holding to achieve the following thing: I want to send data... Show More
shihchinlee
ModusToolbox™ General
I have a design that needs to support USB audio class and an HID generic class simultaneously, are there any examples on USB descriptor design? especi... Show More
Hrithik
Wi-Fi Bluetooth for Linux
Hi Infineon Team,   We are using CYW43455 chip for WiFi in iMX8MM board working on Android 11 OS. We have completed the bringup for WiFi but it is not... Show More
shihchinlee
ModusToolbox™ General
USB_Audio_Device_FreeRTOS sample project of CY8CKIT_062S2_43012 is targeted for AK4954 codec. How to modify the project for WM8960 codec if the mezzan... Show More
NovoNate
PSoC™ 6 SDK
Hello, We are developing a product that contains the CY8C6347 part using ModusToolbox v2.3.1 and we are running into issues when trying to create a bo... Show More
Category Information

Software

Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .