Software Forum Discussions
Browse the Community
ModusToolbox™
The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.
DAVE™
PSoC™ Creator & Designer
Discussion forum regarding PSoC Creator & Designer Software topics.
Wi-Fi Bluetooth for Linux
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).
Featured Discussions
Hi,
Following steps from this discussion: https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Monitor-Mode-Feature-on-CYW43455/td-p/138749, we cannot enable monitor mode od CYW43455.
wl ver
18.15 RC1.67
wl0: Aug 29 2023 01:47:08 version 7.45.265 (28bca26 CY) FWID 01-b677b91b
We're getting error -23 when running wl monitor 1 command:
wl monitor 1
wl: error -23
And also monitor command is not listed in help menu.
Since the wl version is newer than the one in the post is there anything we should do additionally to be able to use monitor mode?
Regards,
Tijana
Show LessHello,
with newer ADS versions, the sync_on_halt.c
file is also being added to the project automatically.
However, it's causing linker errors in some of my projects.
After removing the file from the project, since I am using iSystem for debugging, the linker error disappears.
Show LessHi,
Whenever I open a MTB project, I get a command line terminal getting launched as well. Is there a way to fix this issue? I am using MTB v3.0.
I am attaching the video captured.
Thank you.
Balek
Show LessI cannot complete installation of ModusToolbox. It says that Login is required to complete installation, but login fails. This is with ModusToolbox Setup 1.0, just downloaded.
It says Login session is in progress ... then
Error: Failed to Login: 'Network Error occurred: 'OperationCancelledError"
Why is the login failing and how do I correct this?
Show LessHi Infineon.
I think that Modus supports double of data type(double precision floating point number type).
Which file in Modus defines about double?
Is double defined in GCC's library?
It would be helpful if infineon could tell me where it is specifically defined.
Best Regards.
YuMa
Show LessHi,
Per Amazon doc, CYW943907AEVAL1F is not supported by many of the libraries required for full IoT functionality.
Primarily I'm talking about OTA
Is there any example project/tutorial demonstring how OTA can be performed using the AWS cloud service?
Same question goes for other IoT related services such as security, TCP etc.
Thanks
Show LessI am writing a program for a BLE HID device and I want to call the functions in the file mtb_shared/btstack/release-v3.8.2/wiced_include/wiced_bt_hidd_ble.h but they are only declarations and not definitions, and I can't call them, is it that I am missing to download some source files?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/ModusToolbox/modustoolbox-%E7%9A%84shared%E5%BA%93%E4%B8%ADbtstack%E4%B8%AD%E7%9A%84wiced-bt-hidd-ble-h%E5%A4%B4%E6%96%87%E4%BB%B6%E4%B8%AD%E7%9A%84%E5%87%BD%E6%95%B0%E6%B2%A1%E6%9C%89%E5%AE%9A%E4%B9%89-%E6%97%A0%E6%B3%95%E8%A2%AB%E8%B0%83%E7%94%A8/td-p/705540
Show LessHello,
I'm currently working with the CYBT-343026-01 Bluetooth module in my custom PCB design, using a dedicated MCU as the host. I've successfully sent the HCI_RESET command [01 03 0C 00] through HCI UART and received the expected response [04 0E 04 01 03 0C 00].
The goal is to establish Serial Port Profile (SPP) communication from MCU to PC via CYBT-343026-01. However, I am uncertain about the next steps for using the module, and I have the following questions:
- Should I enter the application mode or use Bluetooth HCI Mode Interface?
- How to enter the application mode? Should I follow one of the 2 sequences bellow?
Sequence 1:
- Generate application: Use the ModusToolbox to create the .hex file from the RFCOMM-SPP example.
- Program the module: Use WICED Module Programmer to program the module through a USB-to-UART bridge.
- Run the MCU: Start with “CTS is high after the reset” to “apply any stored configuration”
Sequence 2:
- Generate application: Use the ModusToolbox to create the .hex file from the RFCOMM-SPP example.
- Run the MCU: Start with CTS low after the reset to enter download mode
- Program the module: Follow the "Downloading an application to serial flash" procedure described in AIROC™ HCI UART Control Protocol.
I appreciate any guidance you can share. Thank you in advance for your assistance!
Show Lesswhen I read the register of CHIPCOMMON_SR_CONTROL1 to check if the firmware initialized sr engine, it failed, so I wondered how to enable or disable the sr feature, or the firmware initialize the sr feature itself?
Show LessI've recently acquired the solar-powered IoT device kit S6SAE101A00SA1002, and while attempting to operate it in PSoC Creator, I've encountered an issue. Specifically, I couldn't find any package related to solar-powered devices within the software. Upon further investigation on the official website, it became apparent that I need to download the "solarpowerediotsetuponlypackage" tailored for the S6SAE101A00SA1002 device. Could you kindly guide me on where to find and download this package?
Show Less