Software Forum Discussions
Browse the Community
ModusToolbox™
The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.
DAVE™
PSoC™ Creator & Designer
Discussion forum regarding PSoC Creator & Designer Software topics.
Wi-Fi Bluetooth for Linux
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).
Recent discussions
Hi ,
We are having existing project which was created using Wiced Smart IDE for CYW43907 Soc. We are planing to migrate the existing project from Wiced IDE to ModusToolBox. I have installed "ModusToolbox_3.0.0.9369-windows-install" version. Please let me know Is there any step by step migration guide for the same. What would be easy and Quickway to do the same?
Thanks ,
Lokraj
__PRESENT
Show LessHi,
As title. How to build ClientControl source code in WICED Studio SDK??
If anyway to modify and build custom ClientControl tool based on code in WICED Studio?
Thanks.
Austin
Show LessHello
I would like to download the program for CYBT-353027-EVAL and I have installed the following
WICED Studio 6.6
WICED Smart SDK 2.2.3
Platform files for CYBT-353027
But it seems that the Platform files only support the old version of the project folder - 20706-A2_Bluetooth, I try to download the sample program Hello_Sensor under WICED Smart SDK and it will report an error (as shown in the picture).
Thanks
你好
我想对CYBT-353027-EVAL开发套件进行烧录,我安装了以下
- WICED Studio 6.6
- WICED Smart SDK 2.2.3
- Platform files for CYBT-353027
但貌似Platform files只支持老版本的项目文件夹 - 20706-A2_Bluetooth,我 在WICED Smart SDK 下尝试烧录示例程序Hello_Sensor就会报错(如图)。
请问有什么解决办法?
祝好
Yaodong
Show Less
Hi,
I am trying to integrate external SPI Flash Memory to Aurix TC38A (Tricore) controller using IfxQspi driver (version : iLLD_1_0_1_4_0)
1) I could not read the device ID when I am sending the read command (RDID command --> 9Fh )
2) Also the chip select pin is not going low during transmission of the data
Can you please tell me if there is any driver I have to use ? or What am I missing .
Please help me to resolve this issue
Show LessHi, I'm Dwi Wahyudi
I just realize that my laptop has a lot of windows driver package (while cleaning my win10), but I don't know the function of all those driver.
So, can someone tell me what are those driver and can I uninstalled all of those or should I save just one driver?
btw, I only use PSoC CY8CKIT-044 for my project and now i'm done with the project.
Thanks.
Dears
I am not able to show / expanded view of some elements in Search window using mouse lick on "► symbol "
But using +/- keys it is working normally I am able to collapse or expand selected node.
I hope that it could be problem in Eclipse GUI or something else...
Radim
Show LessHi,
I'm looking for the C build settings but it seems I have to add my settings through Makefile. Why we don't have visual Build Settings for the C complier in 2022 like in other eclipse based tools?
Show Less
I'm working on a project with a CYBLE-416045-02 ...and to put it mildly it's very resource limited: I need almost all the pins for some function.
Now I've tried to auto assign all pins ... and the PSoC Creator fails to find a suitalble digital placement.
The question: If the PSoC Creator does not find a suitable digital placement, does this mean that there IS no suitable placement? In other words: Is the search for a solution for the pin assigment complete / exhaustive?
Show LessIn 'Getting started' of ModusToolbox™ Machine Learning user guide ,it tell me install the ModeusToolbox3.0.0 and install ModusToolbox™ Machine Learning pack. I have install MTbox3.0 ,but it is empty that links of ML pack given in the document.
where can find this file?
Show LessPackage Version
ahd-2022_1223
Release Date
2023-01-03
Description
Cypress Android release for the broad market.
This release has been qualified on Hikey 960 platform.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Cypress's connectivity parts.
The release package includes:
* ahd
* device
*hikey960
* firmware
* nvram
* 55572_AndroidBringup.pdf
Test Environment:
* Hikey 960
* 55572 Sanity and VTS
Change Log
[2022-12-23]
* Initial post
Show Less