Software Forum Discussions
Browse the Community
ModusToolbox™
The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.
DAVE™
PSoC™ Creator & Designer
Discussion forum regarding PSoC Creator & Designer Software topics.
Wi-Fi Bluetooth for Linux
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).
Featured Discussions
I am working on cy3214 PSOC eval usb evalution board. I have installed Psoc designer 4.3v. This board uses cy8c24794 IC. I am trying to download a project which is got by installing the designer using Psoc programmer. It is showing that it is connected but when clicked on program it will show busy and fail. it is not getting programmed. so i want a example project built with cy8c24x94 device family and cy8c24794 device.
Thanks and regards Show Less
host require less than 1mA power consumption in idle mode,
and use I2C to control work/idle,
so that, i can't use sleep timer,
because maybe lost wake up command.
Read AN47310, than try analog blocks off,
but... 21434 without ARF_CR,
second try , analog buffer off ,
ABF_CR0 in 21434 without PWR bit .....
Now, my solution is IMO=6MHz,
and CPU_SPEED=SYS_CLK/256,
Please tell me,
how to power off analog block with 21434 ?
What can i do to reduce more power consumption in ilde mode ? Show Less
- Removal of .NET packages from the installer. This has reduced PSoC Programmer download and installer to <30MB.
- Installer tests user's system and, if not in compliance, will prompt the user to install the correct .NET framework (prompt with Microsoft link).
- PSoC Programmer now supports the CY3240 USB-I2C Bridge kit from the COM level.
- Provides hardware access to the CY3240 USB-I2C Bridge through high level API's.
- Expansion of the existing COM level support.
- PSoC Programmer 3.05 now ships with the Clock Programmer. This programmer is built on the PSoC Programmer COM and utilizes the CY3240 USB-I2C Bridge tool to configure Cypress Clock devices. We will continue to expand the Clock support in the future. The user may launch this programmer from the Start Menu > Cypress > Clock Programmer 1.2.
- PSoC Programmer 3.05 also offers a substantial increase in new device support over PSoC Programmer 3.00.0.93. Please see the release notes for a detailed listing of new devices. CY7C604xx, CY7C643xx, CY8C20x36, CY8C20xx6, CY8C22x45, CY8C21x45, CY8C28xxx, CY8CTST201, CY8CTMG201, CY8CTST300, CY8CTMG300, CY8CTMA300, CY8CLED03D0x, CY8CPLCxx, CY8CLED16Pxx.
mov a, REG[PRT2DR]
OR A,0X0FF
MOV REG[PRT1DR],A
but the value at the port is not changing
please do help ASAP
Show Less
When generating the application I get multiple errors and the project is not generated.
In the FunctionParamDecl.h file, lines referring to the valuator look like :
#define ID_pse_valuator_1_m40,00_to_30,00_C_VALUE 0
#define ID_pse_valuator_1_30,00_to_125,00_C_VALUE 1
(etc.)
which are incorrect in C langage (inexpected commas).
This is because the implicit decimal separator used in some non-US countries, e.g. French, is a comma, not a point.
One solution is to make Windows change the implicit decimal separator when running PSoC Designer, but this is tedious and prone to forgetting.
Question : is there a workaround currently available in PSoC Designer ? Show Less
I have been out of the PSoC loop for a while, and want to get started with it again.
Unfortunately I have run into a problem.
I have a PSoC ICE-4000 with USB-4000 usb adapter, which all worked perfectly under designer 4.2
However I now installed (on a new PC) Designer 5.0, which basically seems to refuse to work with anything else than a ICE-CUBE.
After some searching, I have found and installed the PSoC Progammer utility, which enables me to program a PSoC using the ICE-4000. This also works inside Designer 5.0, but I still am unable to select, configure and use the ICE functionality.
Does anyone know how I can get my ICE-4000 up and running under Designer 5.0 ?
Thanks in advance.
Best regards,
Robin Stevenhagen Show Less
What is the deal? Why has it been nuked? Show Less