Software Forum Discussions
Browse the Community
ModusToolbox™
The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.
DAVE™
PSoC™ Creator & Designer
Discussion forum regarding PSoC Creator & Designer Software topics.
Wi-Fi Bluetooth for Linux
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).
Featured Discussions
Hi All ,
I'm new to the wiced SDK . I have upgraded our wiced SDK from 3.6.2 to 6.2. In the old SKD(3.6.2) we writing our bootloader firmware version atthe location 0x004A0000. it is in the ota2_bootloader code and reading this location in the application. We are able to read it. Same thing we did in SDK 6.2, we write boot FW ver to 0x004A0000 location and try to read it. but we are getting 0 value from this location.
How new version affecting the 0x004A0000 location ?
How we can dedug ota2_bootloader code?.
Where i should write version number?
Where i can find memory map with location address.
Please help me to understand it.
Thanks and regards,
Basava.
Show LessDoes it exist Windows 10 drivers for the CYW954907AEVAL1F kit so it can be use as a under windows as a WIFI Station ?
If yes what WICED application needs to be download in the device ?
Regards
Rohde & Schwarz
Jean-Marie Gayet
Show LessIt is my first time using the software and I am having issues with the port selection.No ports are showing up in the 'Port Selection' to program even though my device is connected to my PCs USB port. Any help?
Show LessHi
I used the following method:
1. Press and hold the Recovery button (SW3).
2. Press and hold the Reset (SW2) button for 1 second.
3. Release SW2.
4. Release SW3.
But the board can't to be recovered, the user application previously running again after released SW3.
Which one can tell me what caused this?Thank!
Below is the application program:
void application_start(void)
{
/* Initialize the transport configuration */
wiced_transport_init( &transport_cfg );
/* Initialize Transport Buffer Pool */
transport_pool = wiced_transport_create_buffer_pool ( TRANS_UART_BUFFER_SIZE, TRANS_UART_BUFFER_COUNT );
#if ((defined WICED_BT_TRACE_ENABLE) || (defined HCI_TRACE_OVER_TRANSPORT))
/* Set the Debug UART as WICED_ROUTE_DEBUG_NONE to get rid of prints */
// wiced_set_debug_uart( WICED_ROUTE_DEBUG_NONE );
/* Set Debug UART as WICED_ROUTE_DEBUG_TO_PUART to see debug traces on Peripheral UART (PUART) */
// wiced_set_debug_uart( WICED_ROUTE_DEBUG_TO_PUART );
/* Set the Debug UART as WICED_ROUTE_DEBUG_TO_WICED_UART to send debug strings over the WICED debug interface */
wiced_set_debug_uart( WICED_ROUTE_DEBUG_TO_PUART );//WICED_ROUTE_DEBUG_TO_WICED_UART
wiced_hal_puart_select_uart_pads( WICED_PUART_RXD, WICED_PUART_TXD, 0, 0);
#endif
WICED_BT_TRACE("APP Start\n");
/* Initialize Bluetooth Controller and Host Stack */
wiced_bt_stack_init(hid_audio_management_callback, &wiced_bt_cfg_settings, wiced_bt_cfg_buf_pools);
// wiced_rtos_create_thread();
//ADD
while(1)
{
}
}
Show LessHas anyone successfully coded and ran a SoftAP application on the CY8CPROTO-062-4343W prototype board?
I've tried every possible avenue I can think of to no avail.
Mbed OS 5.12: Negative
WICED Studio 6.2.1: Negative
Modus Toolbox 1.1: Negative
I did manage to get the WiFi scanner sample to work on mbed OS 5.12.2, but that's as close as I could come and this platform clearly can only handle station-mode though I suspect the libwiced_drivers.a library has the function calls, however there are no header files to use them.
I don't see anything in the LBEE5KL1DX data sheet that would indicate it is not capable of being configured as an Access Point. Looks to me to be purely a lack of code. Am I to conclude: This is a homework assignment for the purchaser of these prototyping kits?
This is really frustrating because I can see all the WWD code in WICED Studio that surely should be able to properly communicate with this WiFi chip and configure it as needed. I'm really hoping I'm just missing the obvious here, but so far, nothing but walls.
Show LessGreetings,
I have some problems to make the OTA process in the field.
In two times, during the OTA process, the BCM4343W are rebooting by whachtdog timer. And after try to boot the module again, they don’t work.
The message that appear it’s showing below:
Starting WICED v5.0.0
Started ThreadX v5.6
Initialising NetX_Duo v5.7_sp2
Creating Packet pools
WWD SDIO interface initializing with US/0
Fatal error: download_resource cannot load with invalid size
Could not initialize bus
Could not initialize wifi platform
And the I can’t recover the module.
Clue: "The issue that’s been identified here of two boards getting “bricked”appears to be related to inadequate servicing of the watchdog timer during an OTA update."
Any suggestion to solve this issue?
Thanks in advance!
Show LessHello,
My WICED Expansion for STM (STERLING-LWBTM STM EXPANSION BOARD) doesn't display the JTAG COM port, it only displays the USB -> Serial COM port. I tried reinstalling the driver but it still not working.
The board has the FT2232H chip from FTDI. I checked several discussions about this issue but all of them are old and lack of attachments. Below is my COM port display.
Can any one help me fixing this issue? As far as I know, this issue requires re-programming the FT2232H.
Thank you and best regards,
Duy
Show LessHi expert,
We are using Linux BSA_Server to implement BT Sink function. Application layer uses UIPC_Open to receive PCM/AAC data from BSA_Server.
The data buffer pointer is: pBuffer = ((uint8_t*)(p_msg + 1)) + p_msg->offset;
The data buffer lenght is: p_msg->len
Q1. Is the maximum value of p_msg->len always 1024?
Q2. Where to configure this value or if it's a fixed value and can't be change?
Thanks very much and look forward to your feedback!
Show LessI have 3 BLE devices running simultaneously and pair with indvidual broadcom dongles (client). However the signals keep crossing over and I would like to know where in the code i can assign a dongle and sensor to only pair with each other.
Show Less