Software Forum Discussions
Browse the Community
ModusToolbox™
The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.
DAVE™
PSoC™ Creator & Designer
Discussion forum regarding PSoC Creator & Designer Software topics.
Wi-Fi Bluetooth for Linux
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).
Featured Discussions
Greetings,
I have some problems to make the OTA process in the field.
In two times, during the OTA process, the BCM4343W are rebooting by whachtdog timer. And after try to boot the module again, they don’t work.
The message that appear it’s showing below:
Starting WICED v5.0.0
Started ThreadX v5.6
Initialising NetX_Duo v5.7_sp2
Creating Packet pools
WWD SDIO interface initializing with US/0
Fatal error: download_resource cannot load with invalid size
Could not initialize bus
Could not initialize wifi platform
And the I can’t recover the module.
Clue: "The issue that’s been identified here of two boards getting “bricked”appears to be related to inadequate servicing of the watchdog timer during an OTA update."
Any suggestion to solve this issue?
Thanks in advance!
Show LessHello,
My WICED Expansion for STM (STERLING-LWBTM STM EXPANSION BOARD) doesn't display the JTAG COM port, it only displays the USB -> Serial COM port. I tried reinstalling the driver but it still not working.
The board has the FT2232H chip from FTDI. I checked several discussions about this issue but all of them are old and lack of attachments. Below is my COM port display.
Can any one help me fixing this issue? As far as I know, this issue requires re-programming the FT2232H.
Thank you and best regards,
Duy
Show LessHi expert,
We are using Linux BSA_Server to implement BT Sink function. Application layer uses UIPC_Open to receive PCM/AAC data from BSA_Server.
The data buffer pointer is: pBuffer = ((uint8_t*)(p_msg + 1)) + p_msg->offset;
The data buffer lenght is: p_msg->len
Q1. Is the maximum value of p_msg->len always 1024?
Q2. Where to configure this value or if it's a fixed value and can't be change?
Thanks very much and look forward to your feedback!
Show LessI have 3 BLE devices running simultaneously and pair with indvidual broadcom dongles (client). However the signals keep crossing over and I would like to know where in the code i can assign a dongle and sensor to only pair with each other.
Show LessI am using a PSOC 5 part (CY8C8855) for my first test project (a simple LCD character screen). When I build my project, the build fails and I get the following error:
The command 'arm-none-eabi-gcc.exe' failed with exit code '1'.
How do I fix this error? I am using the latest Beta 5. Show LessWe are using the XMC4700 with a couple of UART apps. One of the parts we are communicating with is a Bluetooth module that requires CTS and RTS for flow control. It does not appear DAVE's UART app has support for this nor can I find any APIs. Has anyone coded this before and be willing to share some code snippets or ideas?
Thanks,
Paul Show Less
Hi,
I wan to realize BLE broadcasts(iBeacon) function and listen function which capturing the location of device embedded CYBT-343026.
I have confirmed the iBeacon function with ezserial_343026-CYBT_343026_EVAL-rom-ram-Wiced-release with SAD command. I can get my customed data in iphone.
But I don't know how to confirm listen function.
"
The scan response packet is transmitted only when a remote device is performing an active scan. During an active
scan, the scanning device send a scan request to any discovered advertising device immediately after receiving the
main advertisement packet. The scan response packet typically includes the friendly name of the advertising device,
and occasionally also includes transmit power, more manufacturer data, or other useful but less critical data that a
remote scanning device may not need to see.
"
I see the function which the spec introduced.
1. Is this the listen function?
2. Could you give me some suggestion for how to realize listen function and confirm it? Is there any related command?
BR,
Treacy
Show Less客户这边需要做一款智能灯,需要支持Sigmesh,支持Homekit的,原厂推荐用CYW20719做的欧司朗智能系列SYLVANIA SMART+产品,欧司朗旗下第一款支持homekit的智能灯泡,详情见下面链接。客户买了两个灯测试过发现仅仅只支持homekit,并不是他们所需要的同时支持homekit+sigmesh的方案。
请帮忙确认下CYW20719是否满足客户同时支持homekit+sigmesh的需求,谢谢!
Show Less