Software Forum Discussions
Browse the Community
ModusToolbox™
The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.
DAVE™
PSoC™ Creator & Designer
Discussion forum regarding PSoC Creator & Designer Software topics.
Wi-Fi Bluetooth for Linux
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).
Featured Discussions
Dear forum,
I have a problem uninstalling Modus Toolbox Software 3.2.0.16028.
The situation:
I installed the ModusToolbox Setup 1.0.0 and Modus Toolbox Dashboard 3.2 from the Infineon website.
However, I had a problem with opening the Eclipse ID because the name of my root folder consists of 2 words with space in between.
So I uninstalled the Dashboard. Doing so I had issues with my antivirus software and the deinstallation.
Any way I changed the name of my root folder not to have a space between the 2 words.
I installed the Modus Toolbox Dashboard.
I still could not access the Eclipse part of the program because it seemed to remember the problem with the root folder name although it had been changed.
I wanted to uninstall the Modus Toolbox Dashboard however, the uninstall software had been deleted by my antivirus for security reasons.
So I am stuck.
Tried uninstalling it from Windows Settings/Apps but was not able. The uninstall icons not clickable.
Do you have a solution or workaround?
Thanks,
Jedison
Show LessPackage Version
ahd-2023_1221
Release Date
2023-12-21
Description
Infineon Android release for the broad market.
This release has been qualified on IMX8 SDIO platform and Hikey960 PCIE platform running Android 13.
Customers wishing to leverage the Android Open Source Platform now have an out of the box Android solution for Infineon's connectivity parts.
The release package includes:
* ahd
* 4373-Android13-SDIO
*43012-Android13-SDIO
*43022-Android13-SDIO
*54591-Android13-PCIE
*55572-Android13-SDIO
*AHDBinaries
*device
*firmware
*nvram
* Android13_55572_SDIO_Release_Notes.pdf
* Infineon_55572_Wi-Fi_6_6E_User_Guide.pdf
* confs
* hostapd_supplicant_src
* Android13_PCIE_Bringup.pdf
* Android13_SDIO_Bringup.pdf
* Android13_Feature_Bringup.pdf
Test Environment:
* IMX8 SDIO setup
* Hikey960 PCIE setup
* 55572, 43012, 43022, 54591 and 4373 Sanity, 6G and 11ax features (55572), WOWL via OOB(55572)
and PNO scan offload(55572, 43022)
Show Lessv5.15.58-2024_0118
Release Date
2024-01-18
Github Link
V5.15.58 backport package: Link
V6.1.19 patch: link
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
Part 1: cypress-fmac-v5.15.58-2023_1128.zip
* Backports package (cypress-backports-v5.15.58-2023_1128-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.15.58-2023_1128.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.15.58-2023_1128.tar.gz)
* Device tree files (cypress-devicetree-2023-11-28.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_10-2023_1128.tar.gz)
* Cypress customer patch (cypress-custom-patch-5.4.21.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Part 2: cypress-patch-v6.1.19-2023_1128.zip
* Cypress fmac patch files for Vanilla v6.1.19(cypress-patch-v6.1.19-2023_1128.tar.gz)
* Infineon-Vanilla-Kernel-v6.1.19-Bring-up-Reference_20201221.pdf
Checksum
cypress-fmac-v5.15.58-2023_1128 sha256sum:
990b5f6beeb9530525f254977569fd25936e09f9ef1bf36ca52118e73dff3e68 cypress-backports-v5.15.58-2023_1128-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
0c8da2efe289115f2242aa3f69de5bc616cb893ecd411e11194c4c008418bb2e cypress-custom-patch-5.4.21.tar.gz
c38cca05bb05db6198af7809c7a2e519cb33a06b02ebd4d626588c9038f7259b cypress-devicetree-2023-11-28.tar.gz
92608ceb4509cc02730833ce2119662b3c116a3956ca303245e97378186dc2a3 cypress-firmware-v5.15.58-2023_1128.tar.gz
771099830bd106307e77ebdd4d27a3e18de27bb60889c4db4bca81f44ade495d cypress-hostap_2_10-2023_1128.tar.gz
8fe7d8b677032fb04374615aae27c5a3131499956dc22ddb420847a3876974c6 cypress-patch-v5.15.58-2023_1128.tar.gz
cypress-patch-v6.1.19-2023_1128 sha256sum:
933ac3a50f0146b4078beb5e398c75a93ab0a1979a93d120a1c0ba2a06ab0ff7 Infineon-Kernel-v6.1.19-Bring-up-Reference.pdf
ac23fabed00e5c5ab0c3720fa0eb6fa135a589e009714f783701fe557abe3fe7 v6.1.19-2023_1128.tar.gz
Part 3: cypress-fmac-v5.15.58-2024_0118.zip
8ccbebf31bf69c85dc7d05fb7e3597fa282c3ba5373d76b2a65364191abb14d0 cypress-backports-v5.15.58-2024_0118-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
92e7196a896fa65138c8297d4202a1811564605360f807faa2c8af310eddeb2e cypress-custom-patch-5.4.21.tar.gz
40dd314cee28149028a2d524ccd5d25f20336c7314e1e26654daecf4c9a796d2 cypress-devicetree-2024-01-18.tar.gz
739d1fae54d885e136847af2957821324c18c68622f204992e268b991172da53 cypress-firmware-2024_0118.tar.gz
2a411fb64818b054498645f64e3ef3b29e4db9a36b65987d9a3af76c2d60f765 cypress-hostap_2_10-2024_0118.tar.gz
8e43bc4487c5d4e77880e2fc9d3152a011063c5b0f3871e277561f0108a88304 cypress-patch-v5.15.58-2024_0118.tar.gz
[Change Log]
2023-12-18 Initial Post
2023-12-22 Add cypress-patch-v6.1.19 to support build brcmfmac on 6.1.19
2024-01-18 Fix for system crash post suspend and resume with CYW55572/55573 [PCIe]
I requested the MCAL for TC37X from Infineon's official website to get a 3-month evaluation version but was rejected to ask me to contact the resellers from the lists listed on the website.
And then I requested from EBTresos website but there is no response after 20 days until now.
And then I got connect with another reseller named Intron, they told me that my case was special and need to discuss with Infineon's guys.
My background is, I want to evaluate my cdd software to check whether it can work well in Infineon's TC375 MCU, and there is no CAR OEM or CAR version. I'm now setting up the environment based on the TC375, and I've already bought the AURIX lite kit V2. I'm wondering if there is no evaluation version I can pay for it, but nobody told me how I can pay, only no response.
What should I do then?
Thanks and Best Regards,
Sunny
Show Less
Hi,
Following steps from this discussion: https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Monitor-Mode-Feature-on-CYW43455/td-p/138749, we cannot enable monitor mode od CYW43455.
wl ver
18.15 RC1.67
wl0: Aug 29 2023 01:47:08 version 7.45.265 (28bca26 CY) FWID 01-b677b91b
We're getting error -23 when running wl monitor 1 command:
wl monitor 1
wl: error -23
And also monitor command is not listed in help menu.
Since the wl version is newer than the one in the post is there anything we should do additionally to be able to use monitor mode?
Regards,
Tijana
Show LessHi all, I am trying to access Modus toolbox 2.4 while connected to my office network. But the performance of the application seems to slower in comparison when connected to mobile hotspot or even without using any internet (No Wi-Fi or LAN cable). To check this issue the office IT team requested these information which I am not able to get. Kindly give your opinion. .The destination IP address of this tool if this is sending any traffic to the Internet. .The port number on which this tool works. Thanks.
Show LessPackage Version
v5.15.58-2023_0901
Release Date
2023-09-01
Description
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.
Files in this release:
* Backports package (cypress-backports-v5.15.58-2023_0901-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.15.58-2023_0901.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.15.58-2023_0901.tar.gz)
* Device tree files (cypress-devicetree-2023-09-01.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_10-2023_0901.tar.gz)
* Cypress customer patch (cypress-custom-patch-5.4.21.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* Documents (docs/)
* README
Checksum
sha256sum:
98d7527606017f851fccb91ef557efaf778c5b2b48264942ed0ea9d7c0a1516a cypress-fmac-v5.15.58-2023_0901.zip
7f88760a74174713d4ffd7aec3479f592c5fa9f876c92941662897454a5feb53 cypress-backports-v5.15.58-2023_0901-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
1a792aa55d847917a7a741418493427ff30dfff10eacf9218b58f192c570942c cypress-custom-patch-5.4.21.tar.gz
1fe05a168cb6e3697e1a7610760f8e86393f53f8fc22b47645b6d00f59365e6d cypress-devicetree-2023-09-01.tar.gz
f0b9d3b25a71b4de69593f511d7e99b49dae8528eb9797983f89f584294963c1 cypress-firmware-v5.15.58-2023_0901.tar.gz
ad057de3baa941ddf59af8b784fe3c3ff1173fe5e04146f07db85362e2d8bb7b cypress-hostap_2_10-2023_0901.tar.gz
96911757cd613afb743db1c504fc3db2184456f3af0d79a814e6463ce384689a cypress-patch-v5.15.58-2023_0901.tar.gz
2023-09-11 Initial Post
- Add 43455 FW
After changing the settings in the configuration wizard, after saving, return to the keil programming interface, and the window will not pop up, which means that the configuration change wizard did not work
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX-Development-Studio/config-Wizard-%E4%B8%8Ekeil%E6%9B%B4%E6%96%B0%E4%B8%8D%E5%90%8C%E6%AD%A5/td-p/685422
Show LessI need two external interrupt in my project and want to use BUTTON1 (P1.14) and BUTTON2 (P1.15) on xmc4500 Relax Kit. I added PIN_INTERRUPT App to Dave CE 4 project. When I try to Manual Pin Allocator for it I see only BUTTON2 in the list. There is not BUTTON1. I checked user manual of xmc4500 and both pin (P1.14 and P1.15) has same Pad Type.
Thank you for your help.
Best regards,
Adem
Show Less