Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Software Forum Discussions

Browse the Community

WICED™ Studio

Discussion forum regarding WICED™ Studio related topics.

60230397 8415

ModusToolbox™

The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.

2801559 1485

AURIX™ Development Studio

The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).

945773 169
filter icon

Featured Discussions

MesihK
Wi-Fi Bluetooth for Linux
Hello, We are using 1YN - CYW43439 with CYW4343A2_001.003.016.0031.0000.1YN.hcd firmware. We are experiencing the following error when we connect mult... Show More
Translation_Bot
ModusToolbox™
Hello, ModusToolbox can't network to download information, using ModusToolbox_URL_Modifier_v1.7(IFX-TEST) didn't solve the problem, and following the ... Show More
PhongLe198
Wi-Fi Bluetooth for Linux
Hi Team, We are finding a way to backport Cypress 4373 wireless chip on hardware with USB interface on linux kernel 4.9, after compiling the drivers w... Show More
jiriv
Wi-Fi Bluetooth for Linux
I have a problem with backported FMAC driver when using SDIO interface.When I try to restart the device, kernel crashes on wifi driver.In backtrace th... Show More
karthikpchetty
ModusToolbox™
Hello,   I see the build warning as below in the latest MTB 3.2 version. Is this an issue that can be fixed by Infineon or else it is upto the ARM? -I... Show More
DoubleLo
Wi-Fi Bluetooth for Linux
Package Version v5.15.58-2023_0801 Release Date 2023-08-01 Description This is Cypress's Linux brcmfmac driver and firmware support packa... Show More
amanning
ModusToolbox™
I have installed ModusToolbox 3.2 and wanted to create my first application using the USB on a XMC4500. But I did not get far as the USB (device or ho... Show More
Anonymous
PSoC™ Creator & Designer
Hi guys,    It would be great if you could update PSoC Creator to be DPI-aware. It's actually really close already, so it shouldn't be too much work! ... Show More
alexfanq
ModusToolbox™
I would like to use Modustoolbox to develop rt thread project and was trying to follow the guide https://community.infineon.com/t5/Knowledge-Base-Articles/Porting-RT-Thread-to-ModusToolbox/ta-p/664401... Show More
MesihK
Wi-Fi Bluetooth for Linux
Hello, I want to read the 1YN Bluetooth transmit power and write to it. How can I do this with the `hcitool`? I'm using CYW4343A2_001.003.016.0031.000... Show More
Category Information

Software

Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .