Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Software Forum Discussions

Browse the Community

ModusToolbox™

The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.

6293512 1233

WICED™ Studio

Discussion forum regarding WICED™ Studio related topics.

37282094 8514

AURIX™ Development Studio

The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).

192126 105

Recent discussions

Sort by:
dari_292216
PSoC™ Creator & Designer
Is there a standalone bootloader host application for download somewhere?  Or do I have to tell others to download the whole Creator software if they ... Show More
HongLI_Guo
AURIX™ Development Studio
Dear all: When the floating point is set to exact mode, The debugging result is as follows, and the value cannot be calculated and displayed normally... Show More
RoRo_3281831
PSoC™ Creator & Designer
We have a custom board with a schematic very similar to the CY8CKIT-142 PSoC 4 BLE Module (the one that comes with the CY8CKIT-042 BLE-A kit).  Other ... Show More
EtienneClm
ModusToolbox™ General
Hi everyone,   I am currently using a CY8C4147AZI-S445 within ModusToolbox 2.4.0.   I would like to use multiple timers during deepsleep at the same t... Show More
austin_h
Wi-Fi Bluetooth for Linux
hi, As title. I studied this thread. https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/is-there-a-cyw43438-driver-version-suitable-for-linux-kernel-3-10/td-p/283304... Show More
tstutter
Wi-Fi Bluetooth for Linux
My setup: - ARM host processor running 5.10 Linux.  - Murata 1MW BT/Wi-Fi combo chip (BCM43455) over SDIO - Wi-Fi firmware: version 7.45.249 - Using l... Show More
Théo
Bluetooth SDK
Hello,   I'm trying to do a sofware reset on a Cypress CYW20721 and I can't find any information about this in the SDK documentation (https://infineon.github.io/btsdk-docs/BT-SDK/20721-B2_Bluetooth/API/index.html... Show More
JWilson
ModusToolbox™ General
Hi  I am struggling with an error message for my CY8CKIT-062-BLE on ModusToolbox When I try and run some code while the board is conneted I get the er... Show More
JuIn_1625121
ModusToolbox™ General
Modus Toolboxを使用してPSoC4100 s maxの設計をする際、 Device configuratorでのDrive modeの設定でinput bufferのOn/Offが選べますが、 AN86439 – PSoC® 4 – Using GPIO Pins記載の下記の図の入力バッ... Show More
tayo
Bluetooth SDK
Hello Infineon support team. We are evaluating CYW920721B2EVK-02 EVB and  would like to set it to sleep mode. Please tell me the reference source code... Show More
Category Information

Software

Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .