Software Forum Discussions
Browse the Community
ModusToolbox™
The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.
DAVE™
PSoC™ Creator & Designer
Discussion forum regarding PSoC Creator & Designer Software topics.
Wi-Fi Bluetooth for Linux
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).
Featured Discussions
Hi, I`m new in DAVE and XMC, just was working with Atmel Studio and AVR before. Could you please help me to figure out why my MultiCAN and Interrupt doesnt work ? I set it with typical settings but nothing happened when I`m trying to recieve a CAN ID 568 data to the node0. If I transmitt a data to node1, the Transmitt function says CAN is BUSY (in debugger mode). At the end it will be the CAN filter for my car navigation.
Thank you !
Show Less
Hi all,
I would like to try the firmware upgrade example for my dev kit. But it is not working.
Can you please advise me what I have wrong?
I am attaching an error log.
PS: I am using latest ModusToolbox v 3.2.
Best Regards
Koumak
Show LessHi Infineon.
PSoC Creator allows flash protection with “Design Wide Resources(Flash Security)”.
Please confirm below figure.
Could you please let us know how to apply protection to flash in Modus?
Target device is PSoC4100S Max
PSoC4100S Max only supports Modus.
Best Regards.
YuMa
Show LessHi Folks,
From the previows discussion, finally I could download Setup1.0
https://community.infineon.com/t5/ModusToolbox/Release-Announcement-ModusToolbox-v3-2-available-for-download/td-p/714363
Then when I tried to ModusToolbox setup, it did not went good.
So I removed related files, as far as I could think of, then re-downloaded
ModusToolboxSetupInstaller_1.0.0.468_windows_x64_signed.exe
launcher2_2023.9.1_Windows_x32-x64.exe
I installed both and in the Launcher I can see the SETUP
In this window, I'm already logged in as me, but allow me to hide my working mail address 😉
(At least "Log out" icon is there)
Then when I click and start the Setup, I get
Error: Failed to start Launcher Service: 'process failed to start'
and
Error: Failed to check for the ModusToolbox Setup update
Since the upper left of the ModusToolbox Setup 1.0 is saying "Login"
I clicked the "Login" Icon, then got
Error: Failed to Login: 'process failed to start'
Note: The right side of the "Login" Icon is saying "Login session is in progress" >_<
Just in case, let me note that I can login to both MyInfineon and IDC.
(1) MyInfineon
(2) Infineon Developer Community (So, I can post this here)
Since the Setup Utility has removed my ModusToolbox 3.1,
currently I have no MTB on my PC, I'd really like to install v3.2.
Now my question is would someone teach me what the safest or the most reliable way to install MTB v3.2 is?
And/or how can I find the cause(s) of errors above?
moto
Show Less
While I attempt to install the software psoc_designer_5.3.exe, error always happens.
Hi everyone,
The PWM App does not allow CCU8 to be selected in DAVE 4.3.2 although the App Help states that CCU8 is an option.
Is this just a documentation error and PWM_CCU8 is to be used instead ?
Thanks very much.
Show LessDear all,
sorry, I need to come back to that issue.
It looks like I couldn't open the discussion from here https://community.infineon.com/t5/AURIX/packed-data-structure-with-TASKING-compiler-possible/td-p/695881 again.
I'm not sure if the proposed solution will work (see below).
struct __packed__
{
char c;
int * i;
} s1;
For me this will generate a struct that is named __packed__ and has an instance that is named s1. I think I realized this when I applied the proposed solution twice in a file. The compiler complains about an already defined struct called __packed__.
The other observation in the post linked above - that it might has differences between command line and not command line complier invocations - I didn't check that so far. Maybe that's the explaination because the linked document in the first post about this issue says that it was introduced with v6.3r1 that is not necessarily the same as delivered with ADS (v1.1r8 Build 22011964).
Maybe someone has more details to add to this. Actually I'm quite surprised that this has not been raised more often because in reading external (sensor) devices it is quite common for me to read them as block and map them onto a packed data structure. I thought switching to the GCC compiler but at least the FreeRTOS port, that I'm somehow depending on, is causing problems there.
Best Regards
Markus
Show LessI'm trying to install ModusToolbox on Linux (Ubuntu 22.04) but I fail to get past the login process.
I originally posted a reply to this thread as it looked similar to my issue but was asked to create a new thread instead.
I downloaded "ModusToolboxSetupInstaller_1.0.0.468_linux_x64.deb" from softwaretools.infineon.com and launched it.
I get the following log messages:
After clicking on "Login" nothing happens and I get the following log:
I don't know how to solve this issue as I don't even see a login prompt. I only get the error "Error: Failed to Login: 'process failed to start'"
Show LessHi, my work computer is not connected to the internet can I still use the Modus Toolbox?
Thank you
Joe
I created a new BSP based on a PSoC4 MAX part (CY8C4148AZI-S558) using the BSP Assistant app. I am attempting to create a new CapSense CSX touchpad application using the Eclipse IDE application wizard. I am able to successfully create the project, but when I attempt to compile I get an error:
#error The CAPSENSE(TM) Configurator requires a newer version of the CAPSENSE(TM) Middleware. Update the CAPSENSE(TM) Middleware in your project
I see in the firmware that the middleware version it is including is 4.0, but I have selected 5.0 in the BSP Assistant Library section:
Any idea what could be going wrong?