Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Software Forum Discussions

Browse the Community

ModusToolbox™

The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.

6274682 1232

WICED™ Studio

Discussion forum regarding WICED™ Studio related topics.

37193988 8513

AURIX™ Development Studio

The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).

187882 104

Recent discussions

Sort by:
forvia
AURIX™ Development Studio

is it possible to use ADS via command line, like "make clean" and and "make all" and so on...

ricardoquesada
ModusToolbox™ General
Hi, I'm using ModusToolbox with PSoC6. I know it is possible to launch the debugger from ModusToolbox IDE, but I need to use it from command line. Any... Show More
smyrnoek
AURIX™ Development Studio
Hi all, I am not sure if I locate this question correctly in this forum, but it is as follows: - for unit testing of our application SW we need to be ... Show More
cteqeu
ModusToolbox™ General
When trying to create a new project I get this error. I think there is something wrong because shouldn't connect this to github.com/infineon... ?   T... Show More
vsnkumar
Studio Bluetooth
Hi,    I'm using Cypress Wiced studio IDE (V 6.2.1.2) for CYBT 343026-01 Bluetooth module. For my requirement, In the Wicked studio IDE,  I'm using on... Show More
DaTr_4751301
Bluetooth SDK
We are working on a bluetooth project using a LAIRD EWB.  The STM32F412v mcu does not contain a LPTIMER.  In working with the CYHAL interface, it appe... Show More
DoubleLo
Wi-Fi Bluetooth for Linux
Package Version ahd-2022_0909 Release Date 2022-09-20 Description Cypress Android release for the broad market. This release has been qualified on Hik... Show More
ravo
PSoC™ 6 SDK
Dears I would like to port application which was developed on CY8CKIT-062-WIFI-BT using  CY8C6247BZI-D54 to CY8C6137BZI-F34. I tried to create custom ... Show More
cedric_roomz
ModusToolbox™ General
Hi,   I'm trying to make a very low power firmware for a cyw43907 board based on the dev kit design. I have some issues finding example and implementi... Show More
JoBr_1593366
PSoC™ Creator & Designer
I tried to replace all the UAC1 descriptors with UAC2 descriptors, but Windows says "This device cannot start. (Code 10)" and tdd.exe says *** ERROR: ... Show More
Category Information

Software

Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .