Software Forum Discussions
Browse the Community
ModusToolbox™
The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.
DAVE™
PSoC™ Creator & Designer
Discussion forum regarding PSoC Creator & Designer Software topics.
Wi-Fi Bluetooth for Linux
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).
Featured Discussions
Hi,
We are evaluating the published system requirments for PSoC Creator and how we can make them more useful. Does anyone actually look at and use this information? If so, which specs are most useful? Does it help to have both minimum and recommended systems? How do you expect us to account for the fact that the requirements are dependent on the size and complexity of your design?
Any thoughts on this would be helpful. Thanks.
Show LessWhat happens is when you try and Generate/Build a current project it fails to either auto assign pins for you or fails to allow you to assign pins.
Show Less
I'm not sure if this should be posted elsewhere but...
Does anyone know of any quaternion libraries or functions geared towards microcontrollers like PSOC5?
It would be nice if Creator came with some extended math libraries for robotics or other 3D applications.
Hi,
you can now find the production release on the Cypress website. No more Creator Beta releases.
http://www.cypress.com/?rID=39551
To check important information such as minimum system requirements, changes to previous releases and more, please read the Release Notes first:
http://www.cypress.com/?docID=23759
This is exciting!
Robert
Show Less In military and medical applications, it is vital to know if the code you are running is what was written. That is why the ECC idea is great. I love that the processor takes care of this issue instead of me having to run a CRC on the Flash at run-time.
I have written a simple piece of code that re-writes an instruction in flash after programming to force a fault. For example, I set up a simple sum in normal code and then switch it to a subtraction afterwards. When I turn on ECC mode, the ECC prevents the switch from occurring (great...ECC works!). I haven't checked, but I imagine the subtract opcode is only 1-bit different from the add opcode. The trouble is I can't figure out how to register the ISR code when a supposed ECC event occurs. I have found allusions to this ability in the PSoC 5 datasheet and in several appnotes, but there are no examples or further information. Does anyone have this working or have any suggestions? My code is shown below. It is a variation on what I found in an application note. I have commented out my attempts at registering the ISR. I tried a system-level interrupt (only available on the ARM) and a regular one.
#include
volatile uint8 a = 5; // don't let the compiler optimize this away
volatile uint8 b = 3; // don't let the compiler optimize this away
volatile uint8 sum; // don't let the compiler optimize this away
/* To find Row number by dividing the address by 256 */
#define ADDRESS_TO_ROW(A) (A / SIZEOF_FLASH_ROW)
/* To find address of next row */
#define ROW_INCREMENT SIZEOF_FLASH_ROW
/* Define PSoC 5 Flash Base */
#define FLASH_BASE CYDEV_FLASH_BASE
/* define the ECC interrupt code */
/*
CY_ISR(ECC_Fault_ISR)
{
LCD_ClearDisplay();
LCD_Position(0,0);
LCD_PrintString("PROG MEM FAULT");
}
*/
void main()
{
/* Array which contains value to be written to the Flash Row */
uint8 rowFinalData[SIZEOF_FLASH_ROW];
/* Temp Buffer for Flash line of code*/
uint8 rowBuffer[SIZEOF_FLASH_ROW SIZEOF_ECC_ROW];
/* Start and end locaton of the concerned data */
uint8 rowDataOffset;
uint16 rowDataEnd;
/* Row address for instruction in flash */
uint16 rowAddress1;
uint16 index1;
uint8 runTwice = 0;
// Various attempts at assigning the ECC ISR to the vector table
//CyIntSetSysVector(1, ECC_Fault_ISR);
//CyIntSetVector(1, ECC_Fault_ISR);
//CyIntSetPriority(1, 3);
//CyIntEnable(1);
/* Start LCD */
LCD_Start();
/* To display demo started */
LCD_Position(0,0);
LCD_PrintString("Flash Mem CRC TST");
LCD_Position(1,0);
LCD_PrintNumber(a);
LCD_PrintString(" ");
LCD_PrintNumber(b);
LCD_PrintString("=");
//CYGlobalIntEnable; /* enable global interrupts */
/* create a label for the difference operation. In GCC, this will also be
the address of the operation. This code is never called after the initial
declaration. The instruction will be copied into the SUM flash location after
to simulate a program memory fault. */
DIFOPERATION:
sum = a - b;
while( runTwice != 2 )
{
/* create a label for the difference operation. In GCC, this will also be
the address of the operation. This instruction will get clobbered in flash
as this code executes. I do not recommend re-writing flash too much as this
will weaken the holding-power of the flash. If you really want to test the
program memory fault code every time, then you will need a seperate label
to copy the code back to it's original state. */
SUMOPERATION:
sum = a b;
LCD_Position(1,0);
LCD_PrintNumber(a);
LCD_PrintString(" ");
LCD_PrintNumber(b);
LCD_PrintString("=");
LCD_PrintNumber(sum);
LCD_PrintString(" a:"); // show address for verification
LCD_PrintHexUint16( &&SUMOPERATION );
LCD_PrintString(" ");
LCD_PrintNumber(runTwice);
CyDelay(2000); // wait 2 seconds
if( runTwice == 0 )
{
/* Get the address where the sine lookup table is stored */
rowAddress1 = (uint16) &&SUMOPERATION;
/* Calculate the row number from the address, which is the remainder of address/256 (max row size) */
rowDataOffset = rowAddress1%SIZEOF_FLASH_ROW;
/* Calculate the starting address of row */
rowAddress1 = rowAddress1 - rowDataOffset;
for(index1 = 0; index1 < SIZEOF_FLASH_ROW; index1 )
{
if ( index1 == rowDataOffset )
{
rowFinalData[index1] = (uint16) (void*)(&&DIFOPERATION); // replace sum operation with difference operation
}
else
{
/* Save the other elements of the flash row in the same position as they were */
rowFinalData[index1] = CY_GET_XTND_REG8((const void *)(FLASH_BASE rowAddress1 index1));
}
}
/* Must get temperature and set a temp buffer first. My understanding is different power is used
to write to the flash depending upon its temperature. */
if(!CySetTemp() && !CySetFlashEEBuffer(rowBuffer))
{
/* Erase and Program the row. */
CyWriteRowData(0, ADDRESS_TO_ROW(rowAddress1), rowFinalData);
}
runTwice = 1;
}
else
{
runTwice = 2;
}
}
while( 1 )
{
/* Never exit */
}
} // end of main()
Hi,
I am working with PSOC5 CY8CKIT-014. At the moment my exmerimental codes are very small <5% of code space. Nevertheless Creator software downloads 1024 blocks. I do not think this is really needed? I there a possibility to download only the needed blocks for faster download?
Thanks!
Christof
Show LessHi, basically i'm designing a capsense button and slider by using CY8C20424. i need to generate a PWM to drive a buzzer, does the psoc designer 5.1 have the PWM generator module? or any other way i can do?
thanks in advance.
Show Less