Software Forum Discussions
Browse the Community
ModusToolbox™
The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.
DAVE™
PSoC™ Creator & Designer
Discussion forum regarding PSoC Creator & Designer Software topics.
Wi-Fi Bluetooth for Linux
AURIX™ Development Studio
The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).
Featured Discussions
I am pleased to announce that starting this week, the Cypress Applications Engineering team will host live, instructor-led, weekly webinars on different PSoC topics! These webinars are free to all of our customers.
We will initially host them at 9:00am (Pacific Time) on Thursdays. Our first one will be this Thursday, May 19th. We will add additional time slots to support different parts of the world.
All webinars will be hosted via WebEx. You can access the webinar from this link. In case anyone has problems with the link, they can always access the meeting by going to http://cypress.webex.com and entering meeting number 498 741 435.
For this week's topic, we will give an overview-level description of the PSoC 3 & PSoC 5 bootloader system, as implemented by PSoC Creator. We'll cover the architecture, how it works, and major features. Then we'll follow up by building a simple demonstration project for the I2C bootloader.
I look forward to seeing you there!
-Bobby
Show LessHi everyone,
I mentioned it on another thread, but I though it deserved its own thread.
It would be great if there were somewhere to share components we've created. People, right now, are creating new peripherals for the PSoC, and each one makes the PSoC a more valuable microcontroller.
Please, please, can Cypress set up some place for people to upload their own components. Perhaps even a forum here would be appropriate. That way, people can comment on the components, and ask for help.
Many thanks
Hugo Elias
Show LessService Pack 1 is available now (May 2011). This is a complete product release that fixes a number of defects in 1.0 Production and adds support for more sophisticated and reliable bootloading. With SP1 you can select bootloader channels at run-time giving you the flexibility to create powerful new bootloading strategies. Plus, you can apply a CRC data integrity check to the downloaded data to make sure the new image arrives safely.
It is available on both PSoC Creator website: www.cypress.com/go/psoccreator, and the PSoC Creator upgrade mananger.
Show LessHi
I am very new to this PSoc Platform. My doubt "is it possible to design a Triangular waveform generator using VDAC without LUT and DMA? If it so how? And how it is possible to generate a negative voltage using VDAC? If anyone know, please tell me that will help me out to finish my project. Thanks in advance.
"The specified part is not loaded in the device library.
Status 0xc00426c0
Subsystem: PSoC Device Editor Engine"
It looks that Designer has the appropriate user modules for the device present in the development board, since I can create a project from scratch and select the proper device and the CSR user module that it needs to use the CapSense features.
But I really would like to be able to open the example projects to study them and use as a learning help. Any help will be welcome. Thanks. Show Less
I've tried installing PSoC Designer 5.1 SP 1.1 and it gets stuck at this point for hours until I give up and cancel. I have done a complete uninstall of PSoC Designer 5.0 and of the aborted 5.1 install, restarted, and still no luck.
The box is running Windows Vista Business x64.
Anybody else had trouble installing this version? Perhaps I should give up and go back to 5.0?
Show LessHey
Is there some way to perform a limited build? For example, sometimes I just want all the generated source and APIs to be updated. At others I only want the arm code compilation step. This could save a lot of time since each of these steps is rather time consuming....
~Abhijit
Show LessHi guys,
Something which I have wished for a couple of times is a logic function which converts an edge into a pulse.
This block could be very simple, taking one input (the edges) and one clock, which defines the length of the output pulse.
When the block sees an edge (can be configured to detect rising, falling or either), it outputs a pulse which lasts as long as one clock cycle.
Many thanks
Hugo Elias
Show Less