Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Software Forum Discussions

Browse the Community

WICED™ Studio

Discussion forum regarding WICED™ Studio related topics.

49855959 8400

ModusToolbox™

The ModusToolbox™ forum includes discussions regarding multi-platform development tools and a comprehensive suite of GitHub-hosted firmware libraries accompanied by thoroughly tested code example applications.

464604 1418

AURIX™ Development Studio

The AURIX™ Development Studio is a free of charge Integrated Development Environment (IDE) for the TriCore™-based AURIX™ microcontroller family. It is a comprehensive development environment, including Eclipse IDE, C-Compiler, Multi-core Debugger, Infineon low-level driver (iLLD), with no time and code-size limitations that enables editing, compiling, and debugging of application code. Combined with numerous code example projects, the IDE can be used to evaluate the powerful architecture of the AURIX™ microcontroller family. It supports Microsoft Windows 10 as a host operating system (OS).

592693 151
filter icon

Featured Discussions

Sort by:
loop_y0u
PSoC™ Creator & Designer
Hi Community,  I'm currently working with CapSense Touch Switch Application. I'm using CY8C4245AXI-483, CY8C4245LTI-M445 MCUs. I want to use an API wi... Show More
Panometric
ModusToolbox™
Recently, I cannot start a debug session, yet I can do the flash operation. I've tried other targets, regenerating launches, and rebooting, and none o... Show More
NXTY_Nishinaga
ModusToolbox™
Hello, I am using the PMG1-S3 evaluation board (CY7113) to run the sample project "USBPD_DRP_EPR" provided on gitHub. When I write and run FW from Mod... Show More
YR1
ModusToolbox™
use example RFCOMM_Serial_Port: change some code: static uint8_t spp_rx_flow_enable = 1; void spp_connection_up_callback(uint16_t handle, uint8_t* b... Show More
Panometric
ModusToolbox™
I was optimistic we might finally have an OTA solution for the CYBLE-046415, but I'm not seeing an answer yet. I made a try at getting this to work, b... Show More
shepdog87
PSoC™ Creator & Designer
Hi, I am following the guide for the DFU applications for PSOC6.  My understanding for this processor (PSOC 61xx) is that it does have 2 cores, but th... Show More
pwlzlw
Wi-Fi Bluetooth for Linux
I have asked about CYW43353 bt host wake here: https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/CYW43353-BT-host-wake-on-LWB5/td-p/471652 T... Show More
Francesco_Lelli
DAVE™
Good morning, I'm trying to configure the POSIF peripheral to read the position from an encoder. I'm facing a problem setting the RUN bit. After I've ... Show More
Assaf
Wi-Fi Bluetooth for Linux
I bought some amount of CYW20719B1 (CYW20719B1KUMLG in specific) for some project I'm working on. I set them on a small board with a UART connection. ... Show More
wisc_ece353
ModusToolbox™
I am trying to tinker with manifests and I am facing an issue where MTB is saving state and the only way that I can get it to work is by restarting my... Show More
Category Information

Software

Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .