Dear Infineon support Team,
I want to replace BTS442 E2 by BTS441RG in one of our products and have following questions:
Most critical for us is the l...
Show More
Dear Infineon support Team,
I want to replace BTS442 E2 by BTS441RG in one of our products and have following questions:
Most critical for us is the lower maximum allowed Vbb (abs.max) which is 63V for BTS442 and only 43V for BTS441.
The datasheet of the BTS441RG recommends for overvoltage protections 150 Ohm between BTS441.GND and Signal GND. I would like to implement these 150 Ohm but am wondering, if there are any further informations about this replacement:
1) do you have some further informations about replacing BTS442 E2 by BTS441RG not written in the datasheet?
2) Any drawbacks i might currently not be aware of using the 150 Ohm resistor for OV protection as proposed in datasheet?
3) is there a LTspice model for BTS441RG available? For example the BTS436L2G has one on your homepage.
Thank you very much in advance for your support!
Best regards,
Bastian
Show Less