Smart Power Switches Forum Discussions
This BTS7004-1EPP, the output is connected to the DC motor driver chip, and then to the motor, in that case, this RGND removed and directly grounded will work, right? Thank you!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E6%99%BA%E8%83%BD%E7%94%B5%E6%BA%90%E5%BC%80%E5%85%B3/7004%E6%8E%A5%E5%9C%B0/td-p/723932
Show Less在哪里索取高边开关芯片的PCB封装?比如BTS7004-1EPP,BTS50060等
谢谢!
How to contact original official Sales of Infineon in China Guangdong Province?
Hello. - Hi! May I ask
1. What exactly is the content of the green module UNDER_VOL_DET ECT ION on the left in Figure 33 of the Annex?
2. What is the specific function of the switching device Q4 in Figure 33 of the Annex?
3. Is there any more detailed information about the planar transformer in this picture? For example, design principle, number of turns, wire diameter, PCB, etc.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E6%99%BA%E8%83%BD%E7%94%B5%E6%BA%90%E5%BC%80%E5%85%B3/%E5%BC%80%E5%85%B3%E7%94%B5%E6%BA%90%E8%AE%BE%E8%AE%A1/td-p/695129
Show LessWhat are the voltage (Vs) and junction temperature (Tj) conditions for the Min and Max values of the IPD kILS parameter?
My understanding is as follows.
Min: Vs=6V, Tj=-40 degrees
Max: Vs=18V, Tj=150 degrees
If my understanding is different, please let me know the correct conditions.
Best Regards,
Tetsuo
DIS pin不管拉High or Low 皆無法控制811G, 試著採用OUT2A & OUT2B 以及 OUT3A & OUT3B有接負載時漏電流準位為1V是否為正常現象!? 無負載漏電流準位為VBB...請問有建議修改的地方.
謝謝
Dear Sir,
BTS7010-1EPA在正常测试过程中器件突然失效,测量Vin脚的电压只有1V,经排查发现IN脚对地电阻只有120K,正常是600K左右。目前在排查失效原因,确认Vin电压未查过限值,Vs电压也是稳定的,工作电流也未超过限值,能否帮忙建议应该从哪些方面去排查,谢谢!
原理图如下:
Show Less
Hi Community
Does anyone have an elegant solution to measuring current on each of the outputs for the TLE9104?
Why HSD fail while driving a Relay?
Hello everyone, i am using STM32F4 to communicate with TLE6232GP to control and diagnostic Oil Control Valve Solenoid.
i have problem i use stm32f4 to output SPI signal and a PWM signal to control Valve, i want to make sure IC TLE6232GP has self-diagnosis function when this valve fails.
Thanks
Show Less